It looks like you are coming from United States, but the current site you have selected to visit is Belize. Do you want to change site?

Yes, please! No, keep me on the current site

Case Studies

Case Studies

  • Mission-critical support: Xylem powers sewage reliability aboard the USS Hornet

    To help address the USS Hornet’s urgent wastewater system needs, a Xylem Goulds Water Technology 1GD51G4AA model grinder pump was recommended to replace the damaged unit that serves one of the ship’s critical onboard sewage tanks. This support provided the museum with a reliable, high-quality replacement that restored confidence in an essential system while easing the financial burden on the nonprofit organization.
  • A Xylem dewatering solution is going strong at an Alliance coal mine six years after installation

    Alliance Resource Partners, L.P. faced a two-pronged water challenge at one of its many underground mines. At the South Mine of the company’s Gibson County Coal in Indiana, solid-laden water needed to be pumped out of the mine, and a dewatering system needed to be installed in an area with limited space. Multiple pumps had to fit into a mine void less than eight feet high with a narrow, 20-foot entry span.
  • Xylem installs a flexible, high-efficiency surface water pumping system

    Delta Sand & Gravel Co., located in Eugene, Oregon, has been providing quality aggregate materials, service and expertise for almost nine decades. The company offers a full line of aggregate products for year-round, all-weather construction and demolition landfill. Xylem has partnered with Delta Sand & Gravel since 2013, to provide holistic water management solutions.
  • Engineering a more efficient way to source and transfer water

    One of the largest global energy exploration companies faced the challenge of drawing source water among the steep slopes of Northern Pennsylvania. The water had to be drawn from a 30-feet deep wet well beside a creek and then pumped 300-feet vertically out of a ravine into the impoundment pond.
  • Aquavar IPC Enclosure

    Whether it is a borehole application requiring outdoor enclosure or surface mount pump and motor requiring a drive to withstand corrosive environment, the IPC has the right solution. Each drive enclosure is constructed to provide a different degree of protection to personnel against access to hazardous parts.
  • Water is gold to Acorn Farms and Goulds Water Technology delivers

    It began as a small nursery providing shade trees and potted nursery products to local customers. Today, Acorn Farms Nursery, Galena, OH is one of the nation’s largest wholesale producers of shade trees and nursery stock, with 800 acres of field stock and another 160 acres of container stock, all located in greenhouses and holding areas that take on the appearance of dense woodlands, where thousands of saplings await delivery to local nurseries.
  • Rodeo’s demands for irrigation and feeding

    Agriculture is by far the largest user of water – up to 70% of all fresh water consumption is for irrigation. Water has many other agricultural purposes such as washing stations, misters, or drinking water for livestock. In fact, horses consume up to 15 gallons of water per day.
  • Pumps built to stand the test of time

    When Paint/Elk Township Sewage Plant installed a Goulds Water Technology submersible effluent pump in the spring of 1991, they would be set for the next two decades.
  • Xylem helps to save the Sphinx and Giza Pyramids

    To solve the groundwater problems, the EAA and United States Agency for International Development created the Pyramids Plateau Groundwater Lowering Project. Hydrotech evaluated the project and selected Xylem’s Goulds Water Technology products as the best solution for the groundwater problem.
  • D&S Pump Supply and Goulds Water Technology keep Quaker Hill Country Club in the green

    Over time, the irrigation, pressure boosting and flow control systems at Quaker Hill Country Club became problematic and the grounds crew was only able to water one green or fairway at a time. The possibility of a pump failure forced the staff to monitor the pump continuously while in operation to ensure they shut it down before it ran dry.
  • It’s elementary – Xylem goes to the ‘head’ of the class

    The best solution for an elementary school in New York was to install two Goulds Water Technology Hydrovar® variable speed frequency drives (VFD) mounted on the existing 5HP SSV Pumps. Selecting this system would provide the constant pressure needed, enhance efficiency, reduce operation and maintenance costs and decrease space requirements.
  • The flushability of flushable wet wipes

    Sales of flushable wipes have increased due to their convenience. But this convenience can come at a high cost as demonstrated in news reports about the detrimental effects these wipes can have on plumbing systems.