It looks like you are coming from United States, but the current site you have selected to visit is Bahrain. Do you want to change sites?

Yes, please. No. Keep me on the current site.

BIB FAQ: Troubleshooting a continuously-operating syrup pump

Leaks, loose connectors, or air in the BIB bag can cause the syrup pump to run nonstop. Here's what to check and how to fix it.

Overview

If you're noticing your BIB syrup pump is running continuously, there are a few things to inspect. Start by checking for leaks. Most leaks are the result of a loose BIB connector. When not seated properly, air can leak into the syrup inlet line through the area between the BIB connector and the attach point on the BIB, allowing the pump to continue to cycle.

Begin by making sure the BIB connector is fully secure and properly in place. If that does not correct the problem, check all clamps and fitting connections, making certain they're tight and leak free.

Check the BIB bag for air or a hole. If you find either, you'll need to replace the bag.

If you've done all this and the problem persists, contact a qualified technician to repair or replace system components as required.