It looks like you are coming from United States, but the current site you have selected to visit is Bahrain. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Case Studies

Case Studies

  • Simplot partners with Xylem on wastewater treatment projects

    The J.R. Simplot Company, commonly referred to as Simplot, is one of the largest privately held food and agribusiness companies. The company is headquartered in Boise, Idaho, USA, but it has operations around the globe, including Portage la Prairie, Manitoba, Canada, and Caldwell, Idaho, USA.
  • Turnkey wastewater treatment plant for juice manufacturer

    A producer of frozen concentrated and chilled citrus juices was in need of building their own wastewater treatment plant due to the publicly owned treatment works (POTW) facility operating at close to capacity. The juice manufacturer chose to take responsibility for their wastewater treatment by having a plant built to meet their requirements. 
  • Valley Queen Cheese Factory chooses the king of wastewater treatment

    The rapidly expanding cheese company’s wastewater treatment issues were limiting its ability to grow. Valley Queen ADI Systems, a leader in anaerobic treatment of dairy processing wastewater, was selected by Valley Queen Cheese Factory to design and build a system to treat its wastewater.
  • Mobile capabilities - treating hexavalent chromium groundwater

    An effective treatment method for chromium (VI) contaminated groundwater is to reduce the chromium (VI), precipitate the new chromium (III) form, and use a flash floc method to capture and filter out the chromium particulates. At a former chromium manufacturing plant site in Jersey City, New Jersey, Xylem and its subsidiaries have used this treatment method since mobilization in late 2011
  • Groundwater remediation system allows construction to continue

    A mid-Atlantic environmental firm contacted Carbonair to develop a groundwater remediation treatment system for a Brownfield development project. Three office complexes were being built in downtown Washington DC. Each building included underground parking, requiring excavation 65 feet below grade.
  • Meeting effluent discharge requirements for an auto auction facility

    Xylem was approached by a Massachusetts auto auction facility for assistance in meeting discharge requirements for zinc to the Publicly Owned Treatment Works (POTW). Effluent from the facility fluctuated from 6–10 ppm, significantly above the required 1 ppm limit. Additionally, this waste stream contained surfactants and oil which was difficult to treat with a typical ion exchange media.
  • Better disinfection control for aquatic center

    Oregon City Swimming Pool is located in the Portland Oregon metro area. The facility is unique as it has a 200,000 gallon indoor pool and a seasonal 50,000 gallon outdoor wading pool. The wading pool is supplied with water from the indoor swimming pool, necessitating a need for a higher residual in the summer months. 
  • Economic savings achieved with DEPOLOX® Pool E 700 P Controller

    The outdoor aquatic facility Fuldatal in Germany has been a popular destination for more than 40 years. In addition to a lap pool and wading pool, the facility has a diving and a baby pool as well as an enclosed area that features a lazy river. The facility is open daily from May through September and is the perfect aquatic venue for the whole family during the summer months. Although well-liked by its patrons the facility was not a profitable venture in recent years and some cost cutting measures needed to be put in place.
  • Xylem enhances pool safety and security for Berliner Bäder-Betriebe

    For decades, the BBB has relied on Xylem’s proven Wallace & Tiernan® technology for the treatment of its pool water. As a result of its trust in the brand, that has grown over time, Xylem was the first point of contact for the BBB when it came to selecting this new safety technology.
  • Xylem helps to preserve an icon

    Isambard Kingdom Brunel was one of the greatest British engineers of the 19th century. His railways, bridges, tunnels and dockyards still stand as memorials, but his ship, the SS Great Britain, was his innovative masterpiece. When she was launched in 1843 her size, power and innovative technology, including the 1000HP steam engine driving a screw propeller, changed shipbuilding for ever.
  • Xylem reduces pool combined chlorine

    The Bay & Basin Aquatic Centre serves the population of nearby towns, Huskisson and Vincentia which are located between Sydney and Canberra. It features a separate indoor 25 m lap pool and leisure pool with water slide and spas in a modern building nestled in a beautiful bushland setting typical for Australia. As is common in indoor pools of this kind, using sand filtration and liquid chlorine sterilization, the combined chlorine levels built up over time and became resilient to any attempt to remove them.
  • Refinery meets discharge requirements for permit violations

    A Southern California petroleum refinery faced stormwater discharge permit violations for hydrocarbons and heavy metals with a five-day compliance deadline. Xylem rapidly deployed a multi-stage vessel-based system using organoclay, carbon, and ion exchange resins to achieve ppb-level discharge limits, eliminate violations, and restore regulatory compliance within the required timeframe.
  • Pipeline hydrostatic test water treatment equipment rental

    Carbonair was hired by a pipeline operator to provide on-site treatment of water generated by a hydrotest on a section of pipeline. The mobile water treatment system had to be designed to treat suspended solids, oil and grease, and needed to handle a flow rate of 1000 gpm.
  • Groundwater treatment system rental for subsurface pipeline repair

    Carbonair was hired by a petroleum pipeline company to assist in the clean-up and repair of a ruptured petroleum pipeline in South Carolina. The project involved providing temporary treatment of contaminated groundwater generated as a result of dewatering associated with the repair of the ruptured line.
  • Paving the way to environmental responsibility at Shankus Water Park & Resort

    Shankus Water Park is one of India’s largest water parks, spread over 200 acres with a 25-year brand legacy. The water park features the highest standard water rides designed by global leader WhiteWater, Canada, with park operations planned by Forrec, Canada and many other leading global specialists. Shankus Water Park has a strong in-house operations team with vast national and international industry experience.
  • UV solution mitigates microbiological corrosion for CEMEX

    Xylem was approached by CEMEX UK to supply a containerized ATG™ UV wastewater treatment plant to disinfect 125 m3/hr of effluent wastewater which would protect against the microbial induced corrosion of their pipe work and equipment.
  • ConAgra foods selects ADI-BVF® reactor to meet discharge limits

    ConAgra Foods chose ADI Systems' anaerobic technology to treat the wastewater at its production plant. Based on its many years of experience in the food processing industry, ADI Systems proposed its low-rate anaerobic ADI-BVF® reactor to treat ConAgra’s wastewater.