It looks like you are coming from United States, but the current site you have selected to visit is Bahrain. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Evaluating Fine Filtration for Cooling Tower Water Applications

Evoqua’s cross-flow microsand filtration technology applauded In Eneref Institute Cooling Tower report

Eneref Institute has strongly recommended cross-flow microsand filtration technology as the most reliable and efficient technology to eliminate fine particulate (down to submicron particles) in HVAC cooling tower and process cooling applications. Eneref Institute is a research and advocacy organization for sustainable development with an initiative to inspire solutions that promise an earth-friendly economy through socially responsible sustainable development.

As described in the Eneref Report, the system's high efficiency lies in the unique use of microsand and cross-flow filtration. Vortisand® cross-flow filtration systems can capture particles under 1 micron in size, 10 to 50 times smaller than particles retained by traditional media filters. It is a high capacity media filter that combines cross-flow dynamics with microsand media to achieve submicron filtration performance.

The Eneref Report looks at the benefits of cross-flow microsand filtration technology “due to its high-value results and effectiveness at keeping cooling towers clean.” Traditional deep-bed multimedia systems leave unchecked all submicron particles—the particulates that are most responsible for the fouling that supports Legionella growth and system inefficiency.

"We examined the Vortisand system because a better understanding of water filtration systems will help building operators reduce the quantity of toxic chemicals discharged into the environment. Water is a precious and vital resource of our ecosystems on which all life itself is based."

--Seth Warren Rose, Founding Director of Eneref Institute