Documents
-
-
Hot to cold, from start to finish
Our technology plays a key part in managing water delivery through all elements of the HVAC cycle. The products can be categorised into those best suited to commercial applications and those for domestic and residential use.
-
-
-
Hydrosurveyor Enables Rapid Indian Railways Bridge Surveys
The HydroSurveyor-M9 system from SonTek, a Xylem brand, is an instrument/technology that Indian Railway has employed to rapidly measure bathymetry data along with velocity data.
-
Improving aerobic sludge digestion efficiency
The aerobic sludge digester cells at the Langley Wastewater Treatment Plant required major overhaul. This was due to limited capacity, sludge overspray from surface aerators and icing conditions that resulted in shutdown. To tackle these challenges, Xylem recommended easy-to-install Flygt jet aerators to boost process efficiency and meet regulatory requirements.
-
-
Industrial wastewater treatment with low profile air strippers
Industrial process and wastewater can contain volatile organic compounds (VOCS) that can have a negative effect on the production process or downstream wastewater treatment processes. In these instances, it is often necessary to put treatment equipment in place to remove the VOCs.
-
Innovative cover installed for waste-to-energy purposes
LaForge Bioenvironmental operates a waste-to-energy facility in a northwest farming community of New Brunswick, Canada. The system is located on a 1,000 acre (405 hectare) mixed farming operation, which includes the LaForge Holsteins dairy.
-
Installation of online water quality monitoring systems enabled Thames Water to protect a key clean water treatment works from four separate catchment pollution incidents
Online water quality monitoring systems were deployed to protect treatment processes, improve resilience and ensure availability of clean water to the customers supplies.
-
Intelligent pumping supports United Utilities' CSO programme
Xylem and United Utilities collaborated to transition 330 sites to just three standardized pump types, simplifying maintenance and cutting inventory by 85%. This smart network rollout also slashes reactive service calls by over 90% while lowering energy consumption by up to 40%. -
Ion exchange services remove groundwater contaminants
California Water Service Company had acquired another water company with approximately 100 connections, in Porterville, California, located in a remote agricultural area of the Central Valley. Their annual well testing had shown levels of nitrate at or near the Maximum Contamination Level (MCL) of 45 ppm and perchlorate was found in the groundwater at levels above the Public Health Goal (PHG) of 10 ppb. A treatment system was needed to remove both these contaminants to ensure quality potable water for the local community.
-
It’s elementary – Xylem goes to the ‘head’ of the class
The best solution for an elementary school in New York was to install two Goulds Water Technology Hydrovar® variable speed frequency drives (VFD) mounted on the existing 5HP SSV Pumps. Selecting this system would provide the constant pressure needed, enhance efficiency, reduce operation and maintenance costs and decrease space requirements.
-
Lowara pumps drive livestock operations
In a major breeding farm from Bergamo, Italy, Rota Guido Srl has installed two reverse osmosis (RO) and ultrafiltration plants that, coupled with a biogas plant ensure local livestock operations are efficient, sanitary and environmentally responsible.
-
-
-
-
-
Kraft Foods achieves excellent nutrient removals
Due to an expansion in potato chip production, the snack food plant required additional wastewater treatment capacity. It needed to be able to meet strict discharge limits for biochemical oxygen demand (BOD), total suspended solids (TSS), ammonia nitrogen (NH3-N), total nitrogen (TN), and total phosphorus (TP) regulations.
-
Landfill leachate treatment system significantly reduces operations cost
The South Central Counties Solid Waste Agency, located in Hopewell, Pennsylvania needed a cost effective, on-site treatment system to treat 12,500 gpd of leachate and allow for future expansion.
-
-
-
Logan Township, NJ expands water reclamation facility
Situated on the banks of the Delaware River, Logan Township, New Jersey has a long history of caring for its watershed and natural environment. In the early 70s, the town designed what has been described as “the nation’s first ecologically planned industrial complex,” Pureland Industrial Complex.
-
Bilge Water Pumping
Bilge water pumping solutions remove unwanted water from boat bilges using electric, manual, and engine-driven pumps designed to support reliable bilge water...