Changing Nutrient Monitoring Forever
EXO NitraLED is the world’s most accessible UV Nitrate sensor, built with state-of-the-art LED technology, for long-term nutrient monitoring.
ProSample for COVID RNA Detection
With 12 programmable settings, users can configure the instrument to collect wastewater samples, which provides the most accurate representation of the residents in the building and the potential presence of COVID-19.
Vertical Profiling Systems (VPS)
5 Deployment Configurations - Ocean, Pontoon, Fixed, Mini and Aerial provide a reliable, fully-automated data collection platform for the early warning of intrusion events for business and environmental critical decision making
ProSolo Optical Dissolved Oxygen Meter
The ProSolo incorporates smart sensor technology that enables sensors to be automatically recognized by the handheld. Additionally, DIGITAL sensors store calibration data, so probe assemblies can be swapped between handhelds without the need for re-calibration.
Featured Products
- EXO NitraLED UV Nitrate Sensor Utilizing state-of-the-art UV LED technology, EXO NitraLEDâ„¢ is an optical nitrate sensor designed...
- EXO Platform EXO2 Multiparameter Sonde YSI EXO2 Multiparameter Water Quality Sonde with 7 sensor ports (including a central wiper port),...
- 2900M Online Monitor & Control System The YSI 2900M Online Monitoring and Control System featuring the YSI Sitini Online Sampler is a key...