-
EMALCSA: implementation of a digital twin to support decision-making in water supply network operations
The Empresa Municipal de Aguas de La Coruña (EMALCSA) manages the water cycle in the city of A Coruña and seven neighboring municipalities, serving a total population of 400,000. The utility collects, treats and distributes over 36 million cubic meters of drinking water to 138,000 customers each year, via a network of over 560 kilometers, 26 storage tanks and six pumping stations. -
Temporary DAF system supports refinery outage
A temporary wastewater treatment system was deployed during a planned outage to support operations while two existing DAF units underwent repair. -
No margin for downtime: Redundant cooling water treatment for a hyperscale data center
A major hyperscale operator launched a new data center campus in Virginia with a clear mandate: design cooling infrastructure to prevent downtime. With high availability requirements and strict discharge constraints, the project team needed a water treatment partner that could deliver quickly, adapt to design changes midstream, and build redundancy into every critical component. -
High performance data center reduces cooling risk with phased water treatment strategy
A global leader in data center infrastructure set out to build a large-scale, high-performance computing campus in South Central U.S. Built for extreme performance— with redundant electrical topologies, full UPS and battery backup, and very high rack densities —the facility required an equally resilient water filtration system to support primary chilled water and adiabatic chiller cooling. With multi‑gigawatt‑scale power capacity, every system had to be engineered around a single imperative: continuous operation. -
ALJARAFESA: Advanced water cycle asset and work order management
Discover how ALJARAFESA modernized water cycle operations with a unified digital platform that connects asset management, maintenance, and leak detection to improve efficiency, responsiveness, and service delivery. -
Orekan (Navarre Regional Government): early warning system to reduce flood risk
The Autonomous Region of Navarre, located in northern Spain, has a surface area of over 10,000 km² and a population of approximately 680,000, concentrated mainly in the Pamplona metropolitan area. It has a highly complex hydrological system, as it is divided between the Ebro River basin, which covers approximately 90% of the region, and the Cantabrian basin, characterized by short, fast-responding basins. -
Secure in-field firmware updates to support more resilient connected products
EU Cyber Resilience Act: Manufacturers must report vulnerabilities from Sept 2026, with full compliance required by Dec 2027 -
CABB: optimization of the primary wastewater network
The Bilbao Bizkaia Water Consortium (CABB) is the public utility responsible for managing the main drinking water and wastewater network in the province of Bizkaia, serving over one million residents through a range of water supply pipelines, sewer networks, and wastewater treatment plants across 97 municipalities. -
EMASESA: implementation of a digital twin to optimize decision-making in drinking water and wastewater management
Implementation of the Xylem Vue platform to optimize management, anticipate events, and improve the efficiency, resilience, and sustainability of the water cycle in Seville. -
Faster draft beer service with Flojet pumps | Bottoms Up System
For GrinOn Industries, creators of the innovative Bottoms Up draft beer dispenser, the goal has always been simple: deliver great beer to people faster, with less waste and zero compromise on quality. -
EMASA: improving water efficiency through smart water balance analysis
EMASA (Empresa Municipal Aguas de Málaga S.A.) is the Malaga City Council’s public utility which has been in charge of managing the entire urban water cycle since 1987. The company serves more than 600,000 residents and supplies approximately 42 hm³ of drinking water. The system operates at a flow rate of up to 2 m³/s, ensuring urban water supply through an extensive pipeline network of around 2,000 km, divided into approximately 240 DMAs (District Metered Areas) and equipped with over 240,000 meters, 170,000 of which are smart devices. -
Gruppo CAP: intelligent water network management through advanced analytics and predictive asset planning
Gruppo CAP deployed Xylem Vue's AI-driven platform to optimize its 6,500 km water network, reducing water losses and improving asset management. -
City of Mesa pinpoints critical leak, avoiding costly delays
Discover how the City of Mesa, Arizona, used Xylem's SmartBall® technology to pinpoint a hard-to-find pipeline leak, safeguarding infrastructure and avoiding costly delays to a transportation project. -
Sörbyvägen Sewage Pumping Station
In conjunction with the expansion of a new pedestrian and cycle path along Route 160, specifically the section between Sörbyvägen and Myggenäs, new water and sewage pipelines were installed. As a vital component of this project, a new sewage pumping station was established to ensure reliable and long-term wastewater management for the area. -
How Fond du Lac turned a nutrient mandate into a smarter operating model
Discover how Fond du Lac met strict phosphorus limits and saved $82K annually by retrofitting with Xylem's biological treatment. Read the case study now. -
Kiski Valley Water Pollution Control Authority: Future-ready wastewater treatment
Discover how Kiski Valley Water Pollution Control Authority upgraded its wastewater treatment system with Sanitaire ICEAS® technology to handle extreme flows, improve efficiency, and protect the Kiski River. -
Regenerative media filter for an outdoor pool
At the Blumenthal outdoor pool in Bremen the Defender regenerative media filter is replacing the outdated, failure-prone open filter system. -
Stadtentwässerung Celle: Wastewater treatment plant process optimization through artificial neural networks
Celle cuts energy consumption by 22% and chemical use by 56% using Xylem Vue WWTP optimization technology, saving tens of thousands of euros annually. -
Powering Singapore’s next generation of semiconductor manufacturing
Xylem delivered a 700 m³/day ultra-pure water system with world-class purity, fast-track execution and built-in capacity for future fab expansion. -
Intake pumping stations P1 and P2 in Kristianstad
As part of Kristianstad Municipality’s investment in a new wastewater treatment plant, construction of two new intake pumping stations – P1 and P2 – began in 2022. The stations play a central role in the facility and are designed to pump wastewater from the trunk sewer network to the new treatment plant. The project was carried out between March 2022 and November 2024. -
Future-proof water supply for the Waldviertel, Austria
EVN Wasser GmbH, the largest water supplier in Lower Austria, implemented a groundbreaking infrastructure project between 2020 and 2025: the new construction of the drinking water Waldviertel pipeline. This 60-kilometre-long main supply pipeline from the Grunddorf/Donaudorf fountain field to Zwettl secures the future supply of high-quality drinking water to around 120,000 inhabitants – an investment in quality of life and future security for an entire region. -
Delivering cost-effective process monitoring for the welding industry
Discover how Sentec engineered a compact, non-intrusive smart connector to digitally transform welding operations. From non-contact wire speed sensing to seamless Bluetooth integration, this case study highlights a scalable solution built for regulation, reliability and industry-wide adoption. -
CCACVI: Acquisition, implementation, hosting and maintenance of a hypervision solution for water and sanitation systems
The French Community of Communes Albères Côte Vermeille Illibéris (CCACVI) is promoting a hypervision project to streamline its water cycle, based on the Xylem Vue platform. -
Innovative water reuse solutions with Xylem’s advanced treatment technology
Learn how Xylem’s Wedeco UV technology helped Los Angeles achieve advanced treatment, regulatory compliance, and 12 MGD of high-quality recycled water at Terminal Island.