-
Electric Generating Station Maximizes Plant Efficiency
Xcel Energy is a leading provider of electricity and natural gas to customers in the Midwestern US. As part of their expansion plans for the Comanche Station, a coal-fired electric generating station located in Pueblo, CO, Xcel Energy contacted Evoqua Water Technologies to explore cost effective solutions for their water treatment needs.
-
Converted Coal Power Plant Updates Intake Water Screens
With regulatory pressure to shutdown coal-powered energy production plants growing, there are several coal-powered plants retiring or converting to natural gas in the next two years. A power plant located in the southern United States needed to replace its traveling water screens as the plant was retiring two of its three coal-powered units and converting the last to natural gas.
-
Complying with the New CCR Regulations
With new federal regulations for flue gas waste and coal combustion residuals (CCR) in effect, energy companies transitioning from coal-fired to gas-fired power generation began to reclaim CCR storage ponds. A power company located in the southeastern U.S. needed a treatment solution that would reduce arsenic and total suspended solids (TSS) in the impounded water...
-
-
-
-
-
-
-
-
-
-
Xylem provides high quality recovered water for printed circuit board washing
A Southeast manufacturer of printed circuit boards for the defense and medical industries was experiencing poor and inconsistent water quality on their board washing process, which utilized a deionization (DI) system from a local water treatment company. The water quality issue was resulting in re-work of off-spec boards, additional labor to re-process boards that failed quality control review, and higher costs overall.
-
Recycling Cadmium Cyanide Rinse Water to Meet Stringent Quality Requirements
When an aerospace structure manufacturer aimed to limit POTW discharge, Evoqua implemented a rinsewater recycling system using ion exchange, reducing manual treatment, lowering costs, and maintaining high-quality standards.
-
Coal Power Utility Meets Updated CCR Regulations
Updated State and Federal environmental regulations led to a shortened project timeline for a facility that needed a Low Volume Wastewater (LVWW) system. Because the regulation prevented the use of the ash impoundment after the deadline, the facility needed to divert all low volume wastewater flows entering the impoundment from the deadline date to the time a permanent LVWW system could be installed and operational.
-
Lower levels of iron in raw water improves mining production
A southern mining company was developing salt dome gas storage facilities that use water to mine salt from the domes shaping them so they can be used to store natural gas inside under high pressures. The raw water used for the mining process contained high levels of iron (5-8 ppm) resulting in equipment fouling and high maintenance costs.
-
Stone Countertop Company Reduces Dewatering Costs
Stone countertop company, Surface Technology, Inc. of Elkridge, Maryland, knew they needed a larger filter press to improve the efficiency of the company's production system and reduce costs. What they didn't know was how the new press was going to improve their whole system.
-
-
Meeting lower discharge limits for cadmium to prevent fines
After new lower discharge limits for cadmium were introduced, a U.S. metal finishing facility providing aerospace and oil industry services reached out to Evoqua for help. Evoqua conducted treatability testing and filtration analysis, then implemented a selective media ion exchange solution using SCU vessels in a worker/polisher configuration to consistently meet strict ppb-level discharge requirements and restore compliance.
-
Recycling Waste Rinsewater Meets Production Needs During Water Shortage
Facing severe water shortages, a PCB manufacturer implemented wastewater ion exchange to recycle rinsewater, ensuring consistent water quality and uninterrupted production.
-
-
Xylem comes to the rescue after fire destroys facility
After an unexpected fire caused extensive damage to their manufacturing facility, a Southeast Aerospace metal finishing company reached out to Xylem for help. Xylem rapidly deployed a turnkey solution, implementing service deionization (SDI) for incoming water and wastewater ion exchange systems to restore treatment capabilities and support continued production during rebuilding.
-
Ion Exchange Service Treats Cadmium Cyanide Rinse Waters
An aerospace manufacturer used ion exchange to treat cadmium cyanide rinse waters, achieving compliance without hazardous chemicals while meeting tight timelines and budget constraints.
-
Groundwater Treatment System Supports Highway Construction
As part of a major highway improvement project, construction dewatering was required in an area in order to pour footings for an overpass. Contaminated water from an adjacent Superfund site was drawn into the dewatering stream, requiring treatment of the contaminated water stream prior to discharge on-site.