It looks like you are coming from United States, but the current site you have selected to visit is Armenia. Do you want to change site?
The Xylem treatment solution will enable the plant to achieve effluent quality that far exceeds local regulatory standards while also delivering maintenance cost savings of approximately 11 percent annually. The improved quality of effluent will mean that wastewater can be reused in a number of applications. In addition, the new solution will reduce the land area required by more than 90 percent, with the additional available land to be used for commercial purposes and to accommodate a water reservoir.
“We are delighted to be partnering with the authorities in Tolu to
develop this innovative solution,” said
The ICEAS secondary wastewater treatment plant will consist of Xylem’s Sanitaire-branded aeration system, decanters, blowers, monitoring, controls and instrumentation. In addition, Xylem’s Wedeco-branded TAK UV disinfection system and Xylem’s Flygt-branded sludge pumps will be installed at the plant.
The new wastewater treatment solution is expected to be operational in
About Xylem
The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all -- that which occurs in nature. For more information, please visit us at www.xyleminc.com
Source:
Xylem
Jennifer Jacob, +1-914-323-5745
Jennifer.Jacob@xyleminc.com