It looks like you are coming from United States, but the current site you have selected to visit is Armenia. Do you want to change site?
“These full-scale tests, carried out over a six month period, clearly
demonstrate the substantial benefits that Xylem can bring to a
wastewater treatment operation,”
Biological-secondary treatment is the most energy-intensive phase in the
wastewater treatment process, with aeration consuming between 25 and 60
percent of the total energy used in a municipal plant.*
The tests were conducted by Xylem at the Sternö municipal wastewater
treatment plant in southern
With the new Xylem system in place, aeration efficiency is almost three times as high in the test line compared to the reference line. The required airflow was reduced by 30 percent and the system pressure was reduced by 15 percent. These savings were gained by combining a more efficient blower, a higher Standard Oxygen Transfer Efficiency (SOTE), a lower headloss and an energy-optimized dissolved oxygen (DO) control and DO profile, as well as more than 40 years of expertise in optimizing wastewater treatment systems.
Click
here for an abstract of the study. A
detailed paper about the trials is available upon request by contacting
*WEF. 2009. MOP No. 32:
**
About Sanitaire
Sanitaire, a Xylem brand, is committed to providing innovative diffused aeration and biological wastewater treatment solutions to help meet the growing challenge of clean water. Installed in thousands of municipal and industry wastewater treatment applications worldwide, Sanitaire equipment and technologies ensure quality, energy efficient and dependable operations. Standard and customized solutions are designed with deep process capability, experience and regulatory insight to meet any demand from design through installation and ownership with integrity. For more information about Sanitaire, visit www.sanitaire.com
About Xylem
Xylem (XYL) is a leading global water technology provider, enabling
customers to transport, treat, test and efficiently use water in public
utility, residential and commercial building services, industrial and
agricultural settings. The company does business in more than 150
countries through a number of market-leading product brands, and its
people bring broad applications expertise with a strong focus on finding
local solutions to the world’s most challenging water and wastewater
problems. Launched in 2011 from the spinoff of the water-related
businesses of
The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all -- that which occurs in nature. For more information, please visit us at www.xyleminc.com.
Source:
for Xylem
Louise Cassidy, +353 (0) 1 678 9333
Cell: +353 (0)
86 383 5727
louise.cassidy@edelman.com