It looks like you are coming from United States, but the current site you have selected to visit is Albania. Do you want to change site?

Yes, please! No, keep me on the current site

EcoTouch Configuration

The unit is connected to this device with RS-485 through the following terminals.

Terminal Description
ST5 pin 5/6 RS-485(A)
ST5 pin 7/8 RS–485(B)
ST5 pin 3/4 GND
ST5 pin 9/10 Termination (120R)

 

Termination must be activated by a wire jumper between ST5 pin 9/10 and ST5 pin 7/8.

  1. On the EcoTouch screen, go to Menu > I/O Setting, page 3.
  2. Click Secure Connect Mode.
  3. Select OFF or Monitor only or Monitor & Control
  4. Press Enter.
  5. Set the communication parameters.
Parameter Setting
Modbus Device Address 1
Baud rate 9600
Parity None
Stop bits 1