It looks like you are coming from United States, but the current site you have selected to visit is Australia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Case Studies & White Papers

Showing 1 – 24 of 200

New Jersey Town Sticks with a Winner

Kearny Municipal Utilities
Kearny, NJ
Challenge In 2004, a major flood severely damaged the station when it submerged the pump controls. Increasing flows also exceeded the facility’s capacity...

Successful Trials with Flygt Adaptive Mixing Technology

City of Albion, MI
Albion, MI, USA
Challenge Albion completed the update of several components of its four-MGD plant in the fall 2017. Afterwards, plant superintendent Kent Phillips became...

OSCAR system DINO controller reduces nutrient return and improves energy efficiency

City of Green Lake Wastewater Treatment Plant
Green Lake, WI
Challenge Faced with rising operating costs due to increasing energy and chemical prices as well as stricter effluent permit limits, many operators and...

Historic Town Remedies FOG Problem, City of Branford, CT

Brandford Water Pollution Control Facility
Brandford, CT
Challenge Among the pump stations managed by Branford is a long-term problematic station located at Burban Street. There were two primary problems at this...

UV System Saves Energy and Reduces Maintenance

French Creek Wastewater Treatment Plant
North Ridgeville, OH
Challenge The WWTP was built in 1975 by the Ohio Water Development Authorities and was purchased from the State of Ohio by the City of North Ridgeville in...

PLC v’s MultiSmart Comparison

The PLC has achieved great success across a wide range of process control applications, including the water/wastewater pump station panel.PLC v’s MultiSmart...

RTU and control in the same device

Many water and wastewater pump stations have a separate control device and RTU. This brief paper examines the reasons behind this choice, and especially...

Benefits of a Modern SCADA Protocol DNP3 vs Modbus

A protocol is simply the rules that govern the data transfer between parts of a control system. Differentprotocols have varying strengths and weaknesses.This...

Maintenance Strategies: Predictive Maintenance vs “Run to Fail”

One of the most common questions from water and wastewater utilities when they are asked about their maintenance practices in lift stations is: “What do other...

MultiTrode transforms the level sensing landscape with environmentally friendly and cost-saving solutions across the UK water industry

UK
Since their arrival into the UK water industry in 2005, Multitrode has transformed the level sensing landscape by introducing innovative, environmentally...

MultiSmart Pump Station Manager in East Bay Regional Park District

USA
The East Bay Regional Park District (EBRPD) is designated a special district by the state of California. It is the largest special district in the United...

Alaskan town installed new Pump Stations and SCADA system

USA
Read the Government Engineering article describing how a historic Alaskan town installed new Pump Stations and SCADA system.

MultiTrode Provides Reliable Stormwater Pump Controls

USA
Zephyrhills is located in Pasco County, on a ridge that divides the Hillsborough River Basin from the Withlacoochee River Basin. Lake Zephyr, an integral part...

How one Florida utility is benefiting from a state-of-the-art management tool

USA
To learn about Royal Palm Beach's SCADA system, read the article. "Now instead of driving to a lift station, the field force can remotely reset a motor and...

The Metropolitan Fire Brigade (Melbourne) – MFB – uses MultiTrode level sensing and control products for many of its fire trucks

AUSTRALIA
The Metropolitan Fire Brigade utilizes Multitrode's Level Sensing Probes to monitor the liquids stored on board the fire trucks in stainless steel or...

Charles Sturt plans wisely for stormy days ahead

AUSTRALIA
The City of Charles Sturt in South Australia has found real operational benefits in using the new web-based PumpView system. And because there was no software...

OSCAR system DINO controller reduces nutrient return and improves energy efficiency

Green Lake Wastewater Treatment Plant
WI, USA
In order to overcome rising operating costs and stricter effluent permit limits, an advanced process control solution was implemented in an aerobic digester in...

Pushed to the limit: Saving energy and improving treatment at high loads

Sweden
An advanced process control system was implemeneted in a highly loaded Sequencing Batch Reactor (SBR) pilot plant in Hammarby Sjöstadsverk, Sweden. It was...

Do more with less: Integrating nutrient removal control improves treatment capacity and efficiency

Green Lake, WI, USA
A plant with a Sequencing Batch Reactor (SBR) in Green Lake, Wisconsin was upgraded with an advanced process control system. By controlling the process in a...

Do more with less: OSCAR System with NURO controller improves treatment capacity at reduced cost

Sweden
An advanced process control system was implemeneted in a Sequencing Batch Reactor (SBR) pilot plant in Hammarby Sjöstadsverk, Sweden. By controlling the...

Optimizing Chemical Dosing Reduces Chemical Use while Meeting Effluent TP Limits

Black River Falls WWTP
WI, USA
Using an online orthophosphate analyzer combined with automated controls helped the Black River Falls Wastewater Treatment Plant reduce chemical consumption...

Deadly Legionnaire’s disease outbreak stopped with the help of Xylem

Germany
When Legionnaire's disease broke out in Warsten, Germany, more than 150 people were infected and two people dies. Xylem was brought in to install a Wedeco...

Smart Biomass Control Saves Energy While Maintaining Treatment Objectives: Results from Hammarby Sjöstadsverk, Sweden

Sweden
A smart biomass control system was implementated at a pilot plant in Hammarby Sjöstadsverk, Sweden. It was shown to automatically maintain the biomass required...

Solids Inventory Management System (SIMS) Controls MLSS Concentrations to Meet Treatment Objectives: Results from Black River Falls, Wisconsin, USA

Black River Falls, WI, USA
The Sanitaire OSCAR process performance optimizer with SIMS controller, implemented at a conventional activated sludge plant in Black River Falls, Wisconsin,...