It looks like you are coming from United States, but the current site you have selected to visit is Europe. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Connecting cable extensions for motor and accessories cables

Motor and accessory cable extensions are available for purchase. They provide an easy plug and play solution for extending cable length.

Because of power losses it is not recommended to connect more than one extension cable.

Do not submerge the connectors under water.

Connecting the motor extension cable

The connection video is shown below, note that when both cables are connected there is a "click" sound:

Connecting the accessory extension cable

Below is the video showing how to connect the extension cable to the dry run protection accessory:

Below is the video showing how to connect the extension cable to the tank full switch accessory:

You may also be interested in:

Function and use of tank full switch

Function and use of dry run protection