It looks like you are coming from United States, but the current site you have selected to visit is Europe. Do you want to change site?

Yes, please! No, keep me on the current site

Remediation System Treats Chromate Contaminated Groundwater

Challenge

City of Colby, Kansas needed to treat chromate contaminated groundwater from the Ogalala drinking water aquifer. Ace Services, a farm implement manufacturing company contaminated the groundwater from inappropriate discharge of their chroming process. The company has since gone out of business and the project is now part of an EPA Superfund Cleanup.

Solution

Evoqua design features once-through ion exchange resin technology. The resulting treated water is pumped directly to the City of Colby potable water system.

A total of six service vessels, two skidded trains in a lead/lag arrangement with the third vessel in standby, each contain 600 cu. ft. of resin. A resin sluicing diaphragm pump and a resin storage/transfer tank is used for removal of the spent resin. Evoqua delivers new resin via tanker, off loads to the storage/transfer tank, and then loads the tanker with the spent resin.

Evoqua service technicians visually inspect the vessel internals prior to installing the fresh resin from the storage tank.

"Our initial goal was to produce drinking water with levels below that of any regulated limit anywhere in the nation. With Evoqua’s lead-lag system we should have no problem."
Norm Labbe, KKWWD Superintendent

Results

Evoqua's contract is the first chromate fixed bed groundwater remediation system used for potable drinking water.

Evoqua's resin exchange system is self-contained, with tankers removing spent and contaminated resins from the site, thereby eliminating concerns of recontamination.

Evoqua also provides environmentally compliant handling and disposal of the spent resins, eliminating the liability for the City of Colby.