It looks like you are coming from United States, but the current site you have selected to visit is Europe. Do you want to change site?

Yes, please! No, keep me on the current site

Case Studies

Case Studies

  • State of the art water treatment technology for a forging works in Saxony, Germany

    Various cooling towers are operated in the water treatment plant at the forge. Disinfection is carried out using expensive biocides, which are also environmentally problematic for rivers when discharged directly. The company was therefore looking for new, efficient and cost-effective disinfection technology to solve these issues.
  • Water reclamation plant effectively reduces chemical usage

    Saint Petersburg, Florida, is home to about 250,000 residents who enjoy "Florida’s Sunshine City" located on Tampa Bay. The city has one of the largest water reuse programs in the country; it serves residential, commercial and industrial customers via a dual municipal distribution system delivering over 37 million gallons of reclaimed water per day (MGD).
  • Xylem provides upgrade and increased capacity after 45 years

    Avon Lake Water Filtration Plant was built in 1926 to serve the city with the capacity of 2 million gallons per day (mgd), producing water for 1,200 people. The city strives to make their drinking water system among the most progressive in the country. Over time the plant’s treatment processes has evolved to improve drinking water quality. The maximum water production capacity recently increased to meet demand...
  • Municipal waterworks ensures compliance with regulations

    The German municipal waterworks SWU Energy provides 162,000 people per day with potable water. This encompasses a distribution system of approximately 760 kilometres in Ulm, Neu-Ulm and the neighboring districts. More than 11 million cubic metres of water per year come from the valleys of Donau and Iller. The sedimentary nature of the region ensures the high quality of the water which is distributed by twelve pumping stations and ten high-level reservoirs.
  • On-site chlorine generation offers city a safe solution

    The city of Scottsdale, Arizona, a community of more than 200,000 residents was historically totally dependent on groundwater resources. By the mid 1980's, the city began putting together a multi-faceted water resource program to provide the community with a long-term sustainable water supply.
  • On-site Electro Chlorination ensures safe disinfection of reservoir potable water for regional community

    Fraser Coast Regional Council (FCRC), through Wide Bay Water (WBW), a commercialized business unit of the Council, maintains numerous water supply schemes throughout the region, including remote reservoirs. Reservoirs offer security of potable water supply to the community despite seasonal demands. Additional chlorination may be required to ensure the Australian Drinking Water Guidelines are met. 
  • Rand Water installs chlorine and ammonia dosing equipment

    Klomac, the Southern African agent for Wallace & Tiernan® products, has successfully completed the supply and installation of chlorine and ammonia dosing equipment at Rand Water’s Mapleton Pumping Station as part of that station’s upgrading and expansion programme. The Wallace and Tiernan equipment includes four Model V2000™ automatic chlorinators rated at 40 kg/h each, four ammonium hydroxide dosing pumps and GMS chlorine gas leak detection equipment.
  • San Diego plant cuts THM levels in half

    The 34 MGD Otay Water Treatment Plant in San Diego, California serves a population of approx. 200,000. The plant receives raw water from two sources - imported water from the Colorado River and runoff from three local reservoirs.
  • SES Water partners with Xylem for gas disinfection solution

    SES Water supplies 160 million litres of clean water daily to over 735,000 people in the UK across parts of Surrey, Kent West Sussex and South London. Westwood Water Treatment Works in Surrey is central to keeping its supply of water safe for local residents.
  • Safety and design are top priorities for water supplier

    The water supply system in Zurich supplies approx. 850,000 people in the city of Zurich and in 67 nearby municipalities with high-quality drinking water at all times. On average, 151,200 m3 of water are consumed each day, the entire water supply network is 1,542 km long (Figures: 2010).
  • Southern California water utility consults Xylem for disinfection of potable water

    Located in Southern California, this water utility uses wells to store water. These same wells are also used for fire protection. which is especially critical during the summer months. The supply covers about 10,000 customer connections with chloraminated water for residual disinfection, with chlorine and ammonia boosting in various locations.
  • Upgrading to a new cost-effective disinfection solution

    The Weaverville Community Services District (CSD) is a publicly owned municipal water agency located in Weaverville, California. The facility needed to retrofit an existing building and switch from a gas feed system to an onsite hypochlorite system. The conversion from gas to hypochlorite is a trend being seen in many Northern California districts as regulations on chlorine gas increase.
  • Water plant removes manganese and improves turbidity

    This 10 million gallons per day drinking water plant gets its raw water source from a 151,000 acre-feet reservoir situated at an elevation of 5430 ft.  The water intake is through a tunnel at a depth of 200 feet.  The intake does not have provisions for the withdrawal of water from multiple levels in the reservoir. 
  • Water plants merged into a united plant with two pumping plants

    Wassergewinnung Essen (WGE) was founded in 2002 as a co-operative group between Essen Public Services and GELSENWASSER. At the Ruhr in Essen, the company is focused on procurement, extraction, treatment and supply of drinking water and then delivering to its partners.
  • German sugar factory controls cooling circuit disinfection

    Südzucker produces 5.4 million tons of sugar a year. Situated in Obrigheim, located in the Palatinate region, the Offstein Sugar Factory is one of the largest and oldest of nine sugar factories in Germany. Yearly, 1.4 to 1.8 million tons of sugar beets are processed. During the harvesting campaign (September to December), this is about 16,000 tons of beets daily - around the clock. Syrup and sugar are produced from the beets.
  • Economic savings achieved with DEPOLOX® Pool E 700 P Controller

    The outdoor aquatic facility Fuldatal in Germany has been a popular destination for more than 40 years. In addition to a lap pool and wading pool, the facility has a diving and a baby pool as well as an enclosed area that features a lazy river. The facility is open daily from May through September and is the perfect aquatic venue for the whole family during the summer months. Although well-liked by its patrons the facility was not a profitable venture in recent years and some cost cutting measures needed to be put in place.
  • Xylem enhances pool safety and security for Berliner Bäder-Betriebe

    For decades, the BBB has relied on Xylem’s proven Wallace & Tiernan® technology for the treatment of its pool water. As a result of its trust in the brand, that has grown over time, Xylem was the first point of contact for the BBB when it came to selecting this new safety technology.
  • Xylem helps to preserve an icon

    Isambard Kingdom Brunel was one of the greatest British engineers of the 19th century. His railways, bridges, tunnels and dockyards still stand as memorials, but his ship, the SS Great Britain, was his innovative masterpiece. When she was launched in 1843 her size, power and innovative technology, including the 1000HP steam engine driving a screw propeller, changed shipbuilding for ever.
  • Xylem reduces pool combined chlorine

    The Bay & Basin Aquatic Centre serves the population of nearby towns, Huskisson and Vincentia which are located between Sydney and Canberra. It features a separate indoor 25 m lap pool and leisure pool with water slide and spas in a modern building nestled in a beautiful bushland setting typical for Australia. As is common in indoor pools of this kind, using sand filtration and liquid chlorine sterilization, the combined chlorine levels built up over time and became resilient to any attempt to remove them.
  • Xylem forges ahead with aluminum cleansing

    Chlorine gas dosing system with double-cylinder connection and automatic compressed gas changeover A-015, two GMS plus gas monitoring systems, Neutralization system, and two cylinder scales.