-
Osby Municipality cuts emergency wastewater pump callouts with Flygt Concertor
Osby was dealing with frequent pump clogs and after-hours callouts. After installing Flygt Concertor, emergency interventions dropped sharply and the team gained more time for planned maintenance. -
Beverage producer scales production through water reuse and recovery
Learn how a California beverage producer supported a 400% production expansion by upgrading its reverse osmosis system, increasing water recovery from 65% to 87%, and reducing wastewater discharge. -
Temporary pumping ensures continuous service during asset replacement
After an unexpected wastewater pump failure, Xylem rapidly installed a temporary NC200 Electric unit integrated with the site’s existing pipework, power and controls to maintain uninterrupted operation during the replacement lead time. Variable speed control and 24/7 Secure Connect monitoring ensured efficient, reliable performance throughout the extended hire period, even when a second pump failed. -
Powering one of India's largest semiconductor manufacturers with Ionpure® CEDI
Discover how Xylem's Ionpure® CEDI solution helped one of India's largest semiconductor manufacturers achieve reliable ultrapure water production with a compact, chemical-free system and more than 45% reduced footprint. -
Loches Sud Touraine cuts pump station maintenance by 90% with Flygt Concertor
Serving 50,000+ residents across a network of 220 pumping stations, Loches Sud Touraine piloted Flygt Concertor at two priority sites—turning frequent clog-related callouts into a scalable upgrade path for the wider region. -
Atlantic Beef Products unlocks growth with wastewater treatment upgrade
Atlantic Beef Products needed more wastewater treatment capacity to support plant growth and the addition of tripe processing. Working with Environmental Industrial Services Inc. (EISI), Xylem modernized the facility's treatment system by implementing membrane bioreactor (MBR) technology and automating key processes while maximizing existing infrastructure. -
Bringing modern efficiency to a historic leisure landmark
Working closely with FT Leisure, Xylem supplied Lowara pumps with integrated Hydrovar X drives, delivering a compact, energy-efficient solution that reduced control panel requirements through pump-mounted variable speed control. The approach simplified system design and installation while helping keep the refurbishment project on schedule. -
Meeting stringent copper discharge requirements in cooling tower blowdown
Xylem delivered a compact, portable ion exchange system with SCU metals-removal media and pre-treatment to reduce copper in cooling tower blowdown to the 0.03 ppm discharge limit. Ongoing AQUA pro service support helps keep the system operating reliably with minimal downtime. -
Rennes Métropole cuts wastewater overflows into the Vilaine River with smart pumping
Rennes Métropole modernized the Constant Véron pumping station upstream of the Beaurade wastewater treatment plant, replacing aging equipment with intelligent Flygt Concertor® pumps. The upgrade increased wet-weather handling and helped prevent overflows to the Vilaine River—delivering higher throughput with stable energy use in the existing footprint. -
Advanced filtration technology transforms Gronau (Leine) outdoor pool in Germany
At the Gronau (Leine) outdoor pool, the forward-thinking and space-saving Defender precoat filter is replacing the old sand filtration systems. -
Friesland Campina simplifies wastewater management with a long-term service agreement
Xylem automates, upgrades and expands key processes and improves effluent quality through a design-build-own-operate agreement -
Intelligent pumping supports United Utilities' CSO programme
Xylem and United Utilities collaborated to transition 330 sites to just three standardized pump types, simplifying maintenance and cutting inventory by 85%. This smart network rollout also slashes reactive service calls by over 90% while lowering energy consumption by up to 40%. -
Lliria Irrigation Association: comprehensive digitization of the irrigation system to improve operational efficiency and resilience
The implementation of an integrated solution, based on the Xylem Vue platform, has enabled the association to transition to digital, centralized, and real-time system management. -
Sustainable ultrapure water for solar manufacturing
A leading solar manufacturing facility in India required a reliable, high-capacity ultrapure water solution to support large-scale production while reducing environmental impact and operational complexity. -
Government of the Principality of Asturias: implementation of a DataHub for regional water cycle management
The solution was set up as a regional DataHub based on the Xylem Vue platform, and provides a comprehensive, centralized view of the regional water cycle to accelerate decision-making. -
CGUCJT: decision-support system for the Jucar-Turia Canal irrigation system
The implementation of Xylem Vue’s Agrotwin platform has enabled the CGUCJT to transition to digital, centralized, real-time management of the Jucar-Turia Canal’s main irrigation water delivery system. -
Brabant Water: end-to-end advanced water supply digitalization using Xylem Vue
Brabant Water deployed Xylem Vue to digitalize its network, integrating data for near real-time operational intelligence and non-revenue water management. -
Rented pump system supports major Scottish Water refurbishment
A temporary pumping system enabled improvements to be completed at a major Scottish Water pumping station, ensuring uninterrupted operation throughout a 10-month project -
Xylem's Orbal® System achieves low nitrate and phosphorus limits in Minnesota town
Minnesota town achieves low nitrate and phosphorus with Orbal® oxidation ditch system -
Temporary bypass solution maintains treatment operations
Discover how Xylem maintained uninterrupted wastewater treatment during critical screw pump maintenance with a compact bypass pumping system, balanced flow distribution, resilient backup power and 24/7 remote monitoring. -
Managing complex temporary bypass flows
Discover how Xylem delivered a resilient temporary bypass pumping solution capable of managing peak flows of up to 500 l/s, maintaining uninterrupted wastewater services and ensuring operational resilience during critical network infrastructure works. -
Keep the greens green: hydrovar® X & the Seneca Falls Country Club
To improve irrigation performance, Seneca Falls Country Club installed three new e-SVX Smart Pumps from Goulds Water Technology. The upgraded system increased pumping capacity from about 400 gallons per minute to approximately 550 gallons per minute, allowing the club to run more irrigation heads simultaneously across the course. -
EnviroMix BioMix minimizes maintenance for WI cheese maker
Read how Mullins Cheese used EnviroMix BioMix™ technology to reduce maintenance, optimize aeration control, and improve mixing efficiency in its wastewater treatment process. -
EnviroMix BioMix provides BNR benefits in Olympia, WA
Read how the LOTT Clean Water Alliance used EnviroMix BioMix™ technology to optimize biological nutrient removal, improve process flexibility, and achieve significant energy savings.