Rainfall and basement areas: how to protect car parks and garages from flooding risks
Even the most efficient drainage systems can be put under strain by exceptional rainfall events. Discover why rapid water removal is essential to limit damage and disruption in residential and commercial buildings.
An increasingly common problem for residential and commercial buildings
Autumn has always been one of the most critical seasons for stormwater management. In recent years, however, the frequency of intense rainfall concentrated over short periods has increased the risk of flooding in many urban areas.
Among the most vulnerable spaces are underground car parks, residential garages, plant rooms, access ramps and basement areas, which are often designed in locations where water naturally tends to accumulate.
When a severe storm exceeds the drainage capacity of existing systems, water can quickly enter below-ground spaces, causing significant financial damage and major disruption for residents, property managers and building operators.
When just a few centimetres of water become a problem
Many people associate flooding with extreme events. In reality, even relatively limited water accumulation can have significant consequences.
In car parks and residential garages, water can:
- render access areas unusable;
- damage cars and motorcycles;
- compromise electrical installations and lighting systems;
- cause water ingress into plant rooms;
- result in costly remediation works.
For condominium managers, property managers and maintenance contractors, rapid intervention is often crucial to limiting damage and restoring normal building operations.
Five good practices to reduce flooding risk in basement areas
While it is not possible to eliminate the risks associated with extreme weather events entirely, several preventive measures can help reduce damage, downtime and restoration costs.
1. Regularly inspect water collection systems
Gullies, catch basins, grates and drainage channels can become obstructed over time due to leaves, debris and sediment. Routine maintenance, especially before the autumn season, helps preserve their efficiency and reduces the risk of water build-up.
2. Pay attention to access ramps
Ramps leading to underground car parks are often the primary entry point for floodwater. Ensuring that drainage and collection systems installed along the route are functioning correctly is essential for intercepting incoming flows from outside.
3. Protect plant rooms and critical infrastructure
Electrical switchboards, fire protection systems, lifts and other critical infrastructure should be adequately protected or located in areas less exposed to flooding risks. Even a few centimetres of water can impair equipment performance, causing service interruptions, damage to installations and costly repair work.
Particular attention should be paid to fire protection plant rooms. Standard UNI 11292 specifies dedicated protective measures when fire pump sets are installed in areas located below street level, requiring suitable systems for managing and removing water in the event of infiltration or flooding, thereby ensuring operational continuity of the equipment even during emergency situations.
4. Establish an emergency response plan
Defining roles, responsibilities and response procedures in advance enables a faster reaction when a critical event occurs. Building managers, maintenance personnel and facility managers should be familiar with the actions to be taken and have access to the necessary equipment.
5. Ensure rapid response capability
When water reaches car parks, garages or basement areas, speed of intervention becomes essential. Having appropriate water removal equipment available can help reduce the time structures are exposed to risk and restore normal operating conditions more quickly.
The role of drainage systems in emergencies
It is not always possible to prevent water ingress completely. Particularly intense weather events, blocked drains, temporarily overloaded collection systems or equipment failures can create unforeseen situations.
In such cases, the availability of reliable drainage systems makes it possible to remove accumulated water quickly and reduce the length of time buildings are exposed to risk.
A rapid response is especially important in buildings where basement areas house essential technical installations or provide the only access route to parking facilities.
Preparing buildings for extreme weather events
Growing climate variability is prompting many property managers and building operators to review their emergency preparedness plans.
In addition to the preventive maintenance of grates, drainage channels and water collection systems, it is important to assess the availability of suitable equipment for rapid intervention whenever required.
Preparation means not only protecting the building and its infrastructure, but also reducing inconvenience for residents, limiting extraordinary costs and improving the overall resilience of the property.
Why practical and easy-to-deploy solutions are needed
During an emergency, simplicity and speed of use can make all the difference.
Maintenance contractors, facility managers and building sector professionals need solutions that can be:
- easily transported to the intervention site;
- installed quickly;
- used in confined spaces;
- relied upon in demanding conditions;
- adapted to multiple application scenarios.
This versatility makes it possible to address different situations, from draining a flooded access ramp to emptying an underground garage or a plant room.