Documents
-
Blog Page
The vital role of UV in optimizing water for microelectronics
Enhancing ultrapure water quality with UV disinfection for microelectronics manufacturing
-
Blog Page
Unmanned offshore platforms: marine growth prevention systems
Reliable, low-maintenance solutions for protecting unmanned offshore platforms from marine growth and downtime
-
Blog Page
Webinar summary: Indirect potable reuse: from concept to demonstration and full-scale implementation
Discover how UK utilities can build confidence in Indirect Potable Reuse (IPR) through continuous verification, advanced monitoring and critical control point frameworks in this Xylem hosted webinar. -
-
A custom bulk dewatering system for 100% compliance
A North American power utility needed to dewater wet fly ash ponds at sites without permanent power. Xylem engineers created a modular system that combined different products into a single streamlined solution.
-
A leader in packaged fruits leverages ozone for maximum disinfection and improved food safety
In the frozen food industry, Listeria is a particularly challenging bacteria as it does not go dormant at low temperatures. Bacterial counts also naturally increase throughout processing and packaging, which requires the operator to closely monitor bacterial levels and conduct complete shutdowns for CIP when necessary.
-
A Xylem dewatering solution is going strong at an Alliance coal mine six years after installation
Alliance Resource Partners, L.P. faced a two-pronged water challenge at one of its many underground mines. At the South Mine of the company’s Gibson County Coal in Indiana, solid-laden water needed to be pumped out of the mine, and a dewatering system needed to be installed in an area with limited space. Multiple pumps had to fit into a mine void less than eight feet high with a narrow, 20-foot entry span.
-
Italian Utility Improves System Reliability and Saves Water, Money and Energy by Locating Water Loss on a Submarine Pipeline
According to Utilitalia, 38 percent of water is lost on average from the country’s distribution networks. By reducing these losses, the country’s utilities can achieve a more sustainable water supply, lower energy demand, and better financial stewardship.
-
Adirondack Beverage installs RO & CDI systems to meet USP regulations
The challenge for Adirondack Beverages was to meet United States Pharmacopeia (USP 23) regulations for the production of bottled water and to be able to meet future USP 24 regulations without additional equipment.
-
Xylem supplies pumps for oil production in West Africa
Several countries and multi-national oil companies are exploiting fields off West African coastlines – including Gabon and Congo – through on-shore plants and off-shore platforms.
-
Ag Processing relies on ADI® MBR for biodiesel wastewater treatment
Ag Processing Inc. (AGP) is a farmer-owned cooperative that processes, markets, and transports grains and grain products. Since its formation in 1983, AGP has grown to include 175 local cooperatives representing over 250,000 farmers throughout the Midwest.
-
-
An underground pump station – fit for a king
Stockholm’s largest pump station is situated some meters below a site which was once a 17th century palace in the middle of the city. The large flows and central location demanded reliable pumps.
-
Anaerobic Technology Eliminates Odor Issues
Headquartered in Mitchelstown, Co. Cork, Ireland, Dairygold’s production facility converts approximately 960 million liters (254 million gallons) of milk annually into top quality dairy products.
-
-
Apă Arieș: Boosting hydraulic performance of the drinking water system
The water and wastewater utility for the Romanian cities of Turda and Campia Turzii, along with 13 other municipalities, Apă Arieș wanted to boost the overall hydraulic performance of their drinking water system to ensure service quality and reduce water loss, especially in rural areas near Turda.
-
App Note: Argonaut-XR Customer Stories
In February 2006 field tests began on the SonTek® Modbus Interface Module (MIM.) These tests were conducted by the Central Arizona Irrigation District (CAIDD) of Eloy, AZ and the USDA’s U.S. Arid-Land Agricultural Research Center from Maricopa, AZ (formerly the U.S. Water Conservation Laboratory in Phoenix).
-
-
App Note: Flowtracker Helps Nepal River Expedition
The Bagmati is both a sacred river and a city sewer, running through Nepal’s capital city of Kathmandu before heading into the mountains and over the Indian border.
-
App Note: Monitoring Coral Reefs in the Caribbean
The Caribbean Community Climate Change Centre (CCCCC) awarded YSI Integrated Systems and Services (a division of Xylem Inc.) a contract
-
App Note: Sontek-IQ Shallow Flow Meter Revolutionizes Flow Measurement in the Australian Bush
It’s hard to picture just how flat Australia’s Murray-Darling Basin is, but picture this – tens of thousands of square kilometers braided with slow-flowing rivers and streams with virtually no fall in their channels.
-
Application of Index Velocity Method in Complex Flow Conditions
Flow monitoring site and hydraulic conditions that can impact a stable stage-discharge relationship comprises of unstable section control, sediment transport, debris, vegetation, off-channel storage, variable backwater effects and unsteady flow conditions.
-
Aquavar IPC Enclosure
Whether it is a borehole application requiring outdoor enclosure or surface mount pump and motor requiring a drive to withstand corrosive environment, the IPC has the right solution. Each drive enclosure is constructed to provide a different degree of protection to personnel against access to hazardous parts.
-