Flygt pumper med kanalpumpehjul

C-3000

PUMPER MED KANALPUMPEHJUL

  • Fås med en enkelt skovl eller flere skovle
  • Traditionelt design med stort gennemløb
  • Højt effektivitet for rent vand
  • Støbejern og valgfri pumpehjulsmaterialer

Har du brug for hjælp?

Kontakt en ekspert
Pumpemodeller Teknologi Kundehistorier & White Papers
Pumpemodeller
Ingen resultater matcher din søgning
Teknologi

FLYGT PUMPER MED KANALPUMPEHJUL

Flygt C-pumperne med kanalpumpehjul er bygget til at kunne håndtere volumener på op til 3.000 l/s med motorer på op til 775 kW.

Basisversionerne af disse pumper er fremstillet af slidstærkt støbejern, og de er beregnet til krævende applikationer, såsom kommunale spildevandssystemer og spildevand fra industrien. Eksplosionssikre versioner er tilgængelige. De klassiske C-pumper med indkapslet pumpehjul med en enkelt skovl eller flere skovle har bevist deres driftssikkerhed igennem årene.

De mindre C-pumper er udstyret med Flygt Nevaclog®-pumpehjul, som har gode egenskaber mht. passage af faste partikler. De større pumper er udstyret med pumpehjul med flere skovle, der giver maksimal hydraulisk effektivitet.

Kundehistorier & White Papers
Circular stormwater pump station

Circular stormwater pump station

FRANCE

Challenge One of the largest airports serving France required a stormwater treatment plant to handle the inflow from a large gravity sewer collecting water from the runways. Solution The pump station...

Læs mere
Pump station with cleaning function

Pump station with cleaning function

SWEDEN

Challenge Eighteen Flygt pump stations transport wastewater at a popular recreational and amusement area in central Stockholm. One of the pump stations handles restaurant wastewater containing fats,...

Læs mere
Expansion of a desalination plant

Expansion of a desalination plant

AUSTRALIA

Challenge One of Australia’s largest cities was running short of fresh water and needed a major expansion of its desalination facility. One hurdle was to transfer the seawater to the plant. A new...

Læs mere
Sewage and stormwater pump stations

Sewage and stormwater pump stations

UK

Challenge The revival of one of Britain’s largest commercially unexploited land areas called for multi-phase construction of two large pump stations. One pump station was to provide drainage for a...

Læs mere
Large capacity circular wet well

Large capacity circular wet well

USA

Challenge Very deep, large capacity and limited footprint: these are common demands by customers for their pump stations designs. Recently, two such pump stations were needed in the US. Solution The...

Læs mere
Circular wastewater lift station

Circular wastewater lift station

USA

Challenge A 54,000-acre service area in a major city in Texas required assistance to handle a projected 50% increase in population and subsequent increase in wastewater processing demands. Solution...

Læs mere
+

There was a problem...

Install for this language not supported at the moment. Please try again later.