It looks like you are coming from United States, but the current site you have selected to visit is Yemen. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Godwin NC150 with Flygt N-technology for sewer pipe cleanout

USA

Brenford Environmental needed to clean more than two miles of 54" (1.4 m) sewer pipe, which had been in place for more than 15 years. The difficult solids in the pipeline included a lot of stringy debris.

Download Case study