It looks like you are coming from United States, but the current site you have selected to visit is Czechia. Do you want to change site?
“Demanding conditions on a worksite and a changed business environment
where resources are limited mean that customers need ever more reliable
and durable technologies, and we are responding to that need with some
smart new dewatering solutions,” said
Xylem’s Flygt BIBO
Xylem’s new Flygt BIBO range incorporates several proven design features taken from the original dewatering pump, as well as innovative enhancements that give the new pumps unmatched wear resistance and uptime capability. Durable and robust, Xylem’s new Flygt BIBO series has been specifically designed for the toughest dewatering environments including mining, quarrying, construction and tunneling. Created by the designers of the world’s most successful submersible drainage pump, Xylem’s new product is a much awaited addition to the company’s product portfolio. More than one million of the original Flygt BIBO pumps have been sold since they were introduced in the 1960s.
Xylem’s Godwin Vac-Prime range
Godwin’s extensive range of Dri-Prime pumps for medium- to high-head applications is now joined by the Godwin Vac-Prime which has been specifically designed for lower-head dewatering jobs. As a result of its compact size, Xylem’s Godwin Vac-Prime is easy to move and transport. It does not require specialist transport and with its lifting frame, fork pockets and optional wheels, it needs minimal on-site equipment. The speed of air evacuation that it delivers is due to a combination of the highly efficient vacuum pump and the fast-priming system. It is light and small in size but has Godwin’s trademark reliability and robustness at its core.
Also on display in Xylem’s booth at Bauma:
Xylem’s Flygt 2600 series
Xylem has enhanced its market-leading Flygt 2600 drainage pump series making it even more reliable and durable, ideal for use in tough dewatering conditions and applications. The Flygt 2600 drainage pumps are at least three times more wear-resistant than conventional drainage pumps*. New enhancements to the range include increased durability of the seal system, greater protection against corrosion, a simplified design and enhanced capability for dry running.
Xylem’s
Featuring non-clog Flygt N-technology, Xylem’s Godwin NC-Series is
engineered to deliver clog-free pumping for maximum uptime and
effectiveness. In sewage bypass and other wastewater pumping
applications, fiber and stringy solids can cause difficulties. Pumps can
often clog, requiring maintenance and resulting in unplanned downtime.
Xylem’s engineering teams in
Xylem is currently expanding its dewatering pump rental offering across
*According to Xylem’s Flygt 100-hour wear test.
About Xylem
The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all -- that which occurs in nature. For more information, please visit us at www.xyleminc.com.
Source:
Louise Cassidy for Xylem
+353 86 383 5727
louise.cassidy@edelman.com
Xylem