It looks like you are coming from United States, but the current site you have selected to visit is Canada. Do you want to change site?
The Plus X Awards is the world’s largest innovation award ceremony for
technology, sport and lifestyle products, and honors manufacturers of
unique, innovative high-quality products. The winners of Plus X Awards
are chosen by an independent, international panel of 25 judges from
various industries. The award ceremony will be broadcast in full on
The Lowara Ecocirc high-efficiency circulator pump, which already complies with the 2015 energy-related products (ErP) directive, was selected for its unique magnetite-resistant “anti-block” technology. This technology completely separates the main flow of the transferred liquid from the permanent magnetic parts, ensuring that the pump is resistant to blockages.
The Ecocirc pump is specifically designed for heating systems in domestic environments. The circulator can reduce electricity costs by up to 90% compared to traditional fixed three-speed pumps, delivering a payback period of just 2-3 years.
“We are honored to win an award of this magnitude,” said
The Lowara Ecocirc previously also received a Plus X Award for innovation, high quality and functionality and the “Best HVAC Marketing Campaign 2013 in Germany.”
About Xylem
The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all -- that which occurs in nature. For more information, please visit us at www.xyleminc.com.
Source:
Xylem Inc.
Jennifer Jacob, +1-914-323-5745
Jennifer.Jacob@xyleminc.com