It looks like you are coming from United States, but the current site you have selected to visit is Hong Kong SAR China. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Xylem to provide sustainable solution for golf course irrigation in Texas

October 6, 2015

OCTOBER 06, 2015

Xylem, (NYSE: XYL), a leading global water technology company dedicated to solving the world's most challenging water issues, has been awarded a $1.25 million contract to provide advanced treatment technology to the South Wastewater Treatment Plant in the city of McAllen, in Texas, USA. The plant provides 240 million gallons of reclaimed, treated wastewater annually to the McAllen Palm View Golf Course for irrigation purposes. Xylem's technology will help to ensure consistent quality at the plant as it treats up to 10 million gallons per day (MGD) of wastewater.

Xylem's Wedeco Duron ultraviolet (UV) system will be used to disinfect the treated plant effluent prior to discharge or reuse. Pathogens potentially harmful to marine life are rendered harmless before the treated wastewater is returned to the environment or used for irrigation. By using UV technology at the plant there is no need to store large quantities of potentially hazardous chlorine on site for effluent disinfection in the city of 130,000 residents. The Wedeco Duron UV system was selected due to its energy efficiency, providing disinfection at the lowest power consumption. Under average flow conditions the system's intelligent autonomous lamp power adjustment and advanced sensor based control features significantly reduces the amount of power required. In addition, Xylem's Flygt Compact Submersible propeller pumps will be used to recycle water in the aeration basins. Using compact, robust direct-drive motors and fewer components, the pumps are designed for efficiency and reliability.

Jay Jordan, Senior Sales Engineer, Xylem said, "We work with customers to ensure plants run at optimum efficiency using sustainable technologies like UV, facilitating maximum water reuse. The fact that our Wedeco Duron system enables the lamps to be easily retrieved for maintenance will significantly reduce maintenance effort of the system. Its extensive performance validation as well as the intelligent autonomous control are crucial factors in meeting permit requirements. Cost-efficient construction costs and ease of installation were also important reasons for selecting our solution."

Xylem's Wedeco (UV) system will help the system to produce 10 MGD of treated water with a peak two hour flow of 31 MGD.  Each UV train will handle 15.5 MGD with a third train providing 50 percent standby capacity.

The installation process at the plant began in March 2015 with the new system expected to be in operation by January 2018. CSA Construction is responsible for upgrading the plant.  

About Xylem

Xylem (XYL) is a leading global water technology provider, enabling customers to transport, treat, test and efficiently use water in public utility, residential and commercial building services, industrial and agricultural settings. The company does business in more than 150 countries through a number of market-leading product brands, and its people bring broad applications expertise with a strong focus on finding local solutions to the world's most challenging water and wastewater problems. Xylem is headquartered in Rye Brook, N.Y., with 2014 revenues of $3.9 billion and approximately 12,500 employees worldwide. Xylem was named to the Dow Jones Sustainability World Index for the last three years for advancing sustainable business practices and solutions worldwide.

The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all -- that which occurs in nature. For more information, please visit www.xyleminc.com.

Xylem