It looks like you are coming from United States, but the current site you have selected to visit is Hong Kong SAR China. Do you want to change site?

Yes, please! No, keep me on the current site

5 ways water utilities can improve financial resilience

5 ways water utilities can improve financial resilience

In times of economic uncertainty, water utilities are challenged to do more with less. It becomes even harder to balance operational requirements with financial sustainability and ratepayer concerns over affordability. Our experts have five tips for how utilities can build financial resilience.
 
New productivity solutions driven by digital technologies can give water utilities bold new ways to optimize their cash flow while maintaining and improving services. These solutions are powered by what Xylem calls Decision Intelligence. This involves using advanced data analytics to help water system operators make the best capital and operating decisions.
 
These solutions have been designed specifically to help utilities increase financial and operational resilience, producing efficiencies over time that can ladder up to major cost savings. If you think they can help you, contact decisionintelligence@xylem.com.

1. Increase revenue without raising rates

A softer economy creates a double whammy: usage often drops, and rate increases become even more challenging to obtain. But what if you could improve cash flow from your existing revenue base without raising rates?
 
Xylem Revenue Locator uses cloud-based data analytics to pinpoint revenue losses from unreliable meters in your metering network, which can add up to a significant lost revenue stream for utilities. It enables utilities to unlock significant hidden revenue without the capital expense of a full-scale meter change-out or a rate increase. The result: improved cash flow without the headache.

$1 million identified
When Clayton County Water Authority in Georgia deployed Xylem Revenue Locator, the utility realized sizable gains. In just over four years, the utility identified over $1 million of recoverable revenue from meter inaccuracies, including those in non-residential meters.

2. Redouble your efforts to reduce energy consumption and third-party costs

Energy is one of the largest non-personnel costs in most water utilities, and new Decision Intelligence technologies can cut energy costs substantially to unlock cash flow. Secondary treatment of wastewater is often the biggest energy user. Xylem Treatment System Optimization uses artificial intelligence to optimize the treatment process, reducing energy costs and freeing up operators to focus on other value-added tasks.
 
In addition, Xylem’s Flygt Concertor, the world’s first wastewater pumping system with built-in intelligence, can reduce the energy consumption of a wastewater pumping station by up to 70%.
 
Plant cuts energy use in wastewater treatment
In Germany, a wastewater treatment plant wanted to reduce energy and chemical consumption while increasing effluent water quality. It used Xylem Treatment System Optimization to predict and calculate the best set points to operate their aerators. The solution reduced aeration energy use by 30%, corresponding to 1.1 million kWh annually – enough energy to power 64 homes for one year.

3. Optimize capital spend by renewing, not replacing assets

Capital budgets come under pressure during periods of slower growth, but the need to keep assets in working order does not go away. One way to stretch budgets without sacrificing operational resilience is to rehabilitate assets instead of replacing them.
 
Large valves are frequently replaced at substantial expense, when many can be rehabilitated to working condition at a fraction of the cost. Pipeline replacement projects often involve digging up and discarding perfectly good pipes. Xylem’s proactive asset management solutions can save millions of dollars by extending the life of their existing infrastructure, enabling utilities to stretch scarce capital dollars.
 
$800,000 saved
A large utility in the Midwest had limited information about which valves in its transmission system required attention and was considering replacing them at a cost of $125,000 per valve. The city decided to have Xylem assess 20 large valves as part of a pilot program. Xylem found that 12 of the valves worked quite well and rehabilitated the other eight to working order, saving the city $800,000.

4. Shrink your capital improvement plan through intelligent optimization

Water utilities often invest millions or billions of dollars in capital improvement projects to expand capacity, in order to comply with regulations and consent decrees, or to create operational headroom. Xylem’s Decision Intelligence approach has shown that utilities can use real-time controls to make better use of their existing systems and reduce the scale of capital improvements needed to achieve their policy objectives.

$1 billion saved
Grand Rapids used Xylem’s visualization and analytics tools to assess planned infiltration and inflow mitigation projects. By linking these to a common analytic framework, the city concluded that many of these projects were not necessary and reduced its capital infrastructure program to less than $50 million, instead of the original $1 billion estimate.

5. Improve efficiency through better workforce management.

Many utilities use enterprise systems that capture high-quality data, but there is no easy way to share it across departments to make more efficient decisions about personnel and assets. Xylem solves this with Kona, a flexible platform for enterprise data integration, work dispatch and mobile field application.

$20 million saved
A large utility in the Rocky Mountain region needed a system that could integrate information between their customer billing system, computerized maintenance management system and GIS to support their staff. Xylem’s Kona platform was deployed to integrate these systems, which increased staff efficiency and reduced IT integration costs, leading to a savings of $20 million over ten years.
 
Save more with Decision Intelligence! Find out how by contacting decisionintelligence@xylem.com.