It looks like you are coming from United States, but the current site you have selected to visit is Jordan. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Osby Municipality cuts emergency wastewater pump callouts with Flygt Concertor

A decade of reliable pumping, fewer callouts, and more time for planned work

Osby Municipality in southern Sweden relies on Skåne Blekinge Vattentjänst AB (SBVT) to operate its water and wastewater infrastructure. Recurring blockages at one wastewater site were creating frequent evening and weekend callouts. In 2016, SBVT turned to Xylem and its intelligent Flygt Concertor® pumping system to solve the problem.

Before Concertor, operators were called out almost every week to deal with pump problems. The pumps had to be lifted for service at least twice a month. Since Concertor was installed in 2016, only one unplanned pump lift has been required in over a decade.

The reduction in emergency work saves around 50 hours of operator time each year.

Challenge

SBVT is jointly owned by four municipalities in southern Sweden — Bromölla, Olofström, Osby and Östra Göinge — and manages water and wastewater services for more than 55,000 residents.

In Osby, SBVT’s responsibilities include five wastewater treatment plants, five drinking-water facilities, and more than 20 wastewater pumping stations. Within that operation, Patrik Nilsson, Operations Supervisor at SBVT, leads a small team that works across both water and wastewater facilities. 

Recurring pump blockages placed a significant burden on the team. At one wastewater pumping station, rags and floor-cleaning mops frequently clogged the pumps and triggered emergency callouts. The operator on call could travel to the site and try to restart the pump, but if it had to be lifted, another employee needed to be called in. It could take around two hours from the initial alarm before the team was able to physically address the problem.

These unplanned interventions were disruptive and expensive, requiring staff time, travel and, when a pump had to be lifted, additional personnel and equipment.

Solution

In 2016, Xylem launched Flygt Concertor, the world’s first wastewater pump with integrated intelligence. Concertor was designed to address exactly this type of wastewater pumping challenge: keeping pumps running in difficult conditions while reducing the need for operators to clear blockages manually. So Xylem recommended that SBVT test it at the site experiencing the most frequent problems.

The new Concertor pump resolved the recurring blockage problem at the pump station, and Osby decided to expand its use of the technology to other locations that had experienced similar problems. The municipality now operates seven Concertor units.

Flygt Concertor is an intelligent submersible wastewater pumping system designed to keep wastewater moving reliably with less operator intervention.

Part of that intelligence is the pump’s ability to detect and respond to potential clogging. Its Adaptive N® hydraulics are designed to resist clogging in the first place. If the system detects a developing blockage, it can initiate an automatic cleaning cycle to help dislodge the material and return the pump to efficient operation. 

Built-in monitoring also records the pump’s operating history, allowing operators in Osby to see when Concertor has triggered a cleaning cycle. This helps them confirm that the pumps are working properly. If several cleaning cycles occur within a short period, the team can arrange to have the pump sump cleaned using a vacuum truck.

Results

Since installing Concertor, Osby has achieved significant improvements in pump reliability, maintenance efficiency, and operational costs:

  • Fewer unplanned pump lifts: Just one in approximately 10 years, compared with at least two per month before Concertor.
  • Reduced emergency callout work: Around 50 fewer hours per year.
  • Lower intervention costs: Fewer costly evening and weekend callouts.
  • Less manual cleaning: Automatic clog detection and cleaning reduce the need to clear pumps manually.
  • Simplified maintenance: Planned annual servicing, with little routine attention required between services.

Reducing reactive maintenance means more than simply avoiding a trip to a site. It gives the operations team more predictable working conditions and more time for planned maintenance and other priorities.

Long-term performance

Osby has relied on Flygt pumps for several decades, and Concertor has now been part of its wastewater operations for around 10 years.

The Concertor pumps receive planned service from Xylem once a year and otherwise require little routine attention from the SBVT team. Instead of repeatedly responding to clogged pumps, operators can rely on the system to identify and address many potential blockages itself.

The result is fewer emergency callouts, less manual maintenance and more productive use of operator time — while helping Osby keep its wastewater infrastructure running reliably year after year.

“You almost forget about the pumps because we don’t have to work on them very much. Once they’re set up and running, we basically don’t have to touch them.”
Patrik Nilsson, Operations Supervisor, SBVT