It looks like you are coming from United States, but the current site you have selected to visit is Europe. Do you want to change site?

Yes, please! No, keep me on the current site

Total water management for chemical processing

How water streams work in a chemical plant

Chemical processing runs on water. Steam production, cooling, process make-up, utility use, product rinsing — every corner of a facility depends on it. So when energy and water costs climb, environmental regulations tighten, and market demand grows, the facilities that stay ahead are the ones that treat water not as a series of isolated problems but as a single, interconnected system. That is the premise of total water management: understanding how each stream flows into the next, and treating the whole cycle as one coordinated operation.

This article is an explainer on how water streams work in a chemical plant. You will learn what each of the four water streams in a chemical plant is — cooling water, boiler feedwater, process water, and wastewater — how they are utilized, and how the water is treated at every stage. We will follow water in the order it moves through the facility, beginning with the largest volume use and ending with the effluent that closes the loop. With a broad range of water treatment technologies and the largest service network in North America, Xylem helps chemical producers minimize risk and downtime, maintain compliance, and reduce operating costs across that entire cycle.

Cooling water

The first place water enters a chemical plant's process is the cooling system, which is also the largest water use by volume in most facilities. Cooling water circulates through heat exchangers and cooling towers to absorb and reject process heat, enabling continuous production and protecting equipment from thermal damage. In chemical plants it is one of the largest water uses by volume, and it presents persistent challenges: dissolved minerals like calcium and magnesium cause scaling on heat-transfer surfaces, suspended solids and biological growth cause fouling, aggressive water chemistry drives corrosion, and warm recirculating water creates a breeding ground for microbes and biofilm. Blowdown — the concentrated stream bled from the tower to control dissolved-solids buildup — also requires treatment before discharge.

Xylem addresses these challenges with a portfolio of disinfection and filtration technologies. On-site electrolytic chlorine generation eliminates hazardous chemical storage while dosing a safe, low-concentration solution for tower disinfection. Ozone generation systems prevent biofilm formation in cooling loops and can even support zero-blowdown operation. Xylem also offers UV disinfection, chlorine dioxide generation, and gas chlorination, plus side-stream and full-flow filtration to control suspended solids. For source-water treatment, ballasted clarification using magnetite accelerates settling and generates cooling water in a compact footprint, and heavy-metal removal media treats cooling-tower blowdown for compliance before discharge.

Boiler feedwater

Once cooling needs are met, the next critical demand is steam — and steam demands the purest water in the plant. Boiler feedwater is the high-purity water used to produce steam for chemical processing. Steam drives reactions, heating, and power generation, and the quality of the feedwater directly determines boiler and steam-turbine efficiency and longevity. Even trace impurities cause serious problems: dissolved minerals produce scale on heating elements that reduces heat transfer and drives up fuel consumption, ionic breakthrough causes pitting of turbine blades, and silica, sodium, chloride, and TOC must be held to very low levels to meet stringent boiler and turbine specifications. Because a feedwater plant must maintain uptime, reliability is as critical as purity.

Xylem provides a full treatment train for boiler feedwater. Reverse osmosis (RO) systems — available in single-pass and two-pass configurations — remove up to 99% of dissolved minerals, paired with softening and multimedia and activated-carbon filtration for pretreatment. For final polishing, continuous electrodeionization (CEDI) produces water up to 18 megohm-cm purity without hazardous regenerant chemicals, using a resin-based membrane process driven by electrical current in a compact, high-flow footprint. Xylem rounds out the offering with ion exchange, degasification, condensate polishing, and mobile RO/demineralization systems for turnarounds and bridge solutions, and brine recovery RO that can recover up to 65% of primary RO waste. For producers who prefer to avoid capital and operational risk, Xylem offers Build-Own-Operate (BOO) models in which Xylem owns and operates the feedwater system for a fixed price.

Process water

Beyond cooling and steam, water is also used directly in the manufacturing process itself — and its purity requirements vary with the application. Process water is water used directly in chemical manufacturing — as process make-up, for utility use, in chemical reactions, and for product rinsing. The water must meet purity standards that vary with the application. Impurities compromise equipment performance and create environmental risk, process water picks up contaminants as it is used, and high-purity water is essential for process and rinsing applications. As production expands and water grows scarcer and more costly, securing reliable process water supply becomes a strategic constraint.

Xylem treats process water with multi-stage trains tailored to the required purity. Reverse osmosis systems generate process water from raw sources, often preceded by media filtration, softening, and high-efficiency pretreatment filtration to reduce silt, and followed by off-site regenerable ion exchange for final purity — a sequence deployed at chemical manufacturing sites producing high-purity process water. Ballasted clarification treats raw river water for industrial use, and membrane filtration and microfiltration softening support water reclaim. Xylem also supplies mobile and temporary treatment systems — demineralization, RO, clarification, and filtration — for interim process water needs.

The most ambitious illustration of total water management is an integrated water-reuse partnership in which Xylem is designing, building, and operating a system that treats river water for cooling and process use while recovering cooling-tower blowdown into demineralized water for boiler feed and process reuse, achieving roughly 90% recovery. For producers who want to shift water treatment off their balance sheet, Xylem offers Water-as-a-Service and long-term design-build-own-operate-maintain (DBOOM) commercial models.

Wastewater

After water has served its purpose in cooling, steam, and process applications, it carries the contaminants it picked up along the way — and that effluent must be treated before discharge or reuse. Wastewater is the effluent generated as water picks up contaminants during chemical production and must be treated to acceptable levels before discharge or reuse. Chemical plant wastewater can contain suspended solids (TSS), fats-oils-grease (FOG), extreme pH, bacteria, selenium, heavy metals, and a range of regulated organic and inorganic substances. Producers face strict pretreatment and direct-discharge limits, municipal surcharges for high-strength effluent, corrosive liquids that demand robust equipment, and — increasingly — Zero Liquid Discharge (ZLD) goals that require near-total water recovery.

Xylem offers end-to-end wastewater treatment. For solids removal, ballasted clarification using magnetite accelerates settling at high rates, and continuous chemical precipitation systems provide skid-mounted treatment with reaction chambers, flocculation, inclined-tube separation, and sludge thickening. A broad family of chemical feed, neutralization, and precipitation systems handles specialized needs: pH control, chemical reaction, chrome reduction, cyanide destruct, and batch treatment, supported by lamella-style clarifiers. For dissolved organics, Xylem supplies activated-carbon adsorption in liquid- and vapor-phase configurations; for heavy metals, specialized removal media and wastewater ion exchange. Biological treatment spans anaerobic digestion (converting waste to biogas) and aerobic treatment with technologies such as oxidation ditches, sequencing batch reactors, and biological nutrient removal. Submersible stainless-steel pumps handle corrosive transport, and digital monitoring provides real-time performance tracking and process optimization. Mobile ballasted-floc clarification can deliver up to 1,000 gpm from a single trailer for spill response.

Together these technologies help chemical producers maintain compliance, avoid surcharges, and move toward water reuse and ZLD.

Build-Own-Operate: water treatment without the burden

Total water management asks producers to think about their water cycle as a whole — but it does not require them to own and run every piece of it. Through Build-Own-Operate (BOO) and broader design-build-own-operate-maintain (DBOOM) models, Xylem takes on the capital investment, design, construction, and day-to-day operation of a treatment system, delivering treated water to the producer for a predictable, fixed price. The customer benefits in several ways at once: no upfront capital expenditure, no equipment on the balance sheet, no in-house staffing or specialized maintenance burden, and guaranteed performance backed by Xylem's service network. Risk — technical, regulatory, and operational — shifts to the partner whose core business is water. The producer gains reliable, compliant water treatment that scales with production, while freeing capital and attention for what actually drives their business: making chemicals. In a total-water-management framework, BOO is the commercial model that makes the integrated vision practical — turning a complex, capital-intensive obligation into a simple, predictable operating cost.