It looks like you are coming from United States, but the current site you have selected to visit is Iraq. Do you want to change sites?

Yes, please. No. Keep me on the current site.

EnviroMix’s BioMix chosen for world’s largest compressed gas mixing installation

Midwest Airport in Indiana

In July 2018, a large midwestern international airport began construction on a stormwater deicing infrastructure project. The project included the construction of three stormwater retention basins each requiring a mixing system.

Midwest Airport in Indiana - BioMix nozzles
BioMix nozzles installed at the floor of each tank provide uniform mixing over a wide range of operating water levels. 

0٫05

HP/1,000 FT3 mixing efficiency

70

% energy savings

Challenge

The equalization basins receive runoff from the airport including the deicing agent propylene glycol. The contents of the basins are eventually sent to the municipal wastewater treatment plant for treatment.  

Due to the extremely high chemical oxygen demand (COD) exerted by the deicing agent, it is critical that the basins be well-mixed in order to prevent major load disruptions at the wastewater treatment plant.

Solution

BioMix Compressed Gas Mixing was selected to provide high efficiency mixing of the three equalization basins with a total combined volume of approximately 100 million gallons — making this the largest compressed gas mixing system in the world!  
With no in-tank moving or wearing parts and non-clog, maintenance free performance, the system allowed the facility to plan for the purchase of a floating cover system in the future, saving an estimated $6 million in construction cost versus a fixed cover to accommodate alternative mechanical mixing technology.

An EnviroMix master control panel (MCP) provides centralized control enabling the automatic adjustment of mixing intensity in all three tanks. High pressure air held in free-standing receiver tanks is optimally distributed to each equalization basin in timed, intermittent bursts through valve modules located adjacent to the tank. 

Midwest Airport in Indiana - largest compressed gas mixing system in the world
With the floor of each basin taking up the space of approximately three football fields, this site is by far the largest compressed gas mixing system operating in the entire world. 

BioMix has no low-level limitations — maintaining the ability to provide superior mixing at any liquid depth — which is of utmost importance in stormwater equalization basins to prevent deposition and maintain homogeneity.  

Most importantly for the airport, BioMix’s bottom-up mixing maintains consistent concentrations of the deicing agent protecting against process upsets at the municipal WWTP that ultimately treats the liquid held in the tanks.

Results

EnviroMix’s patented BioMix technology enables ideal mixed conditions with minimum energy input. BioMix offered monumental energy cost savings for the international airport. The system provides annual energy cost savings of more than $450,000 — equivalent to 70% savings versus conventional mechanical mixing.  

Midwest Airport in Indiana - 3 compressors doing the work of over 40 mixersThree compressors do the work of over 40 mixers from a climate-controlled environment that’s easy to access.