It looks like you are coming from United States, but the current site you have selected to visit is Europe. Do you want to change site?

Yes, please! No, keep me on the current site

How a hyperscale data center protected uptime through resilient cooling water infrastructure

September 3, 2026 Alan Knapp
Industrial Buildings & Facilities Data Centers

A hyperscale data center in Northern Virginia built resilience into its cooling water infrastructure through redundant treatment capacity, helping protect uptime while supporting continuous operations.

Many AI queries, cloud applications and digital transactions depend on one often-overlooked resource: cooling water. As compute density rises and hyperscale campuses expand, the ability to reliably move and treat water is becoming as critical to uptime as power itself. While reliability conversations often focus on power systems, cooling water infrastructure plays a critical role in maintaining uptime, protecting efficiency and supporting long-term resilience.

For a major hyperscale operator building a new campus in Northern Virginia's data center corridor, the mandate was clear from day one: cooling water infrastructure had to support the same uptime requirements as every other mission-critical system. With uptime protection as a priority, the design incorporated redundancy across critical treatment systems to support continuous operations and maintenance flexibility. By reducing single points of failure and enabling maintenance without disrupting cooling operations, resilient cooling water infrastructure can help operators maintain continuity, support compliance and sustain long-term cooling performance.

Why cooling water matters more in the AI era

AI workloads generate significantly higher heat loads than traditional computing environments, increasing dependence on cooling infrastructure. As operators build larger campuses and pursue higher rack densities, water management and treatment systems are becoming strategic assets that help maintain reliability, efficiency and compliance across the facility lifecycle. For hyperscale operators, cooling infrastructure is no longer simply a supporting utility. It is increasingly considered mission-critical infrastructure that directly affects operational performance and business continuity.

Why does cooling water complexity threaten data center operational continuity?

Protecting uptime requires more than delivering enough cooling capacity. Hyperscale operators must also manage increasingly complex cooling water systems that support both cooling performance and environmental compliance. As facilities scale and cooling demand grows, maintaining operational continuity depends on balancing these requirements without creating new operational risks.

The Northern Virginia campus faced a challenge common to large hyperscale developments: managing two separate cooling water streams, each with distinct treatment requirements. One stream supplied cooling tower makeup water drawn from a nearby reservoir. The second handled cooling tower blowdown water that required treatment before discharge to a local creek.

Maintaining cooling tower performance depended on treating the makeup water stream to control suspended solids and iron. Without effective treatment, these materials can contribute to scaling and corrosion that reduce heat-transfer efficiency, increase maintenance requirements and impact long-term cooling performance.

At the same time, the blowdown stream had to meet strict discharge requirements before returning to the environment, including limits on dissolved metals. Consistently meeting those requirements was essential to maintaining compliance and supporting uninterrupted facility operations.

The challenge was not simply managing two treatment processes. It was ensuring both systems could continue operating without interruption. Any component taken offline for service could create unnecessary operational risk if redundancy was not built into the design. For a facility where operational continuity is paramount, the cooling water infrastructure needed to support maintenance flexibility, compliance assurance and reliable performance simultaneously.

Adding complexity, the project was delivered on an accelerated schedule, and design changes introduced during construction required adjustments to the treatment approach without affecting delivery timelines.

How did the operator build resilience into cooling water infrastructure without compromising project timelines?

Working alongside the project's engineering partner, Xylem helped develop a treatment architecture that minimized single points of failure while providing the operational flexibility needed for a rapidly evolving hyperscale campus. From the beginning, the priority was clear: maintain cooling operations during maintenance events, avoid single points of failure and support the facility's uptime requirements across both cooling water streams.

The solution incorporated dedicated treatment systems for both cooling tower makeup water and cooling tower blowdown, allowing each stream to be managed according to its specific water quality and compliance requirements. Parallel filtration capacity and redundant pumping ensured cooling water treatment could continue uninterrupted if a pump required service, a filter vessel was taken offline or other maintenance activities occurred. This reduced operational risk while helping the facility maintain continuous cooling performance.

For the blowdown stream, treatment was designed to support consistent discharge compliance before water returned to the receiving creek. Building compliance into day-to-day operations helped reduce the risk of violations, remediation costs and permit-related disruptions that could affect long-term operations.

Maintaining project momentum was equally important. When the design evolved mid-project and required scope adjustments, Xylem worked with the project team and engineering partner to realign the solution with updated construction requirements while maintaining the original delivery commitment. This flexibility helped keep the project on schedule without compromising the facility's resilience objectives.

To support these goals, the deployment included two Vantage® Pre-Treatment – Industrial (PTI) series multimedia filtration systems engineered to provide automated treatment, operational visibility and continuous performance across both water streams. The pre-engineered and factory-tested design helped streamline installation and startup while supporting long-term cooling water management requirements.

Cooling stays online, discharge stays compliant and the schedule holds

For hyperscale operators, cooling infrastructure is a critical component of operational continuity. The Northern Virginia deployment was designed to ensure cooling water treatment could continue uninterrupted, even when individual system components required maintenance or service.

Today, the Vantage® PTI filtration systems deliver up to 1,200 gpm of treated cooling tower makeup water while maintaining total suspended solids below 20 ppm and dissolved iron below 1 ppm. At the same time, a dedicated treatment stream manages 200 gpm of cooling tower blowdown to meet creek discharge requirements before water returns to the environment.

1,200

Gallons per minute of treated cooling tower makeup water

20

Parts per million or less total suspended solids, with dissolved iron below 1 parts per million

200

Gallons per minute of cooling tower blowdown to meet creek discharge requirements

The most important outcome is resilience. The facility can take individual treatment components offline for maintenance without interrupting cooling water operations. That capability helps reduce single points of failure and supports the uptime requirements associated with mission-critical computing environments. At the same time, the blowdown treatment process maintains compliance performance before water returns to the receiving creek, helping reduce environmental and regulatory risk.

The project team also maintained the original delivery commitment despite mid-project scope changes. By adapting to evolving design requirements without affecting construction timelines, the deployment demonstrated how resilience and schedule certainty can be achieved simultaneously.

Together, these outcomes illustrate how resilient cooling water infrastructure helps hyperscale operators protect uptime, support compliance and maintain operational continuity as compute demand continues to grow. By planning for maintenance, compliance and reliability simultaneously, operators can support long-term campus growth without introducing additional operational risk.

Frequently asked questions

How can hyperscale data centers protect uptime and operational continuity through resilient cooling water infrastructure? Hyperscale data centers protect uptime and operational continuity through cooling water infrastructure that incorporates redundancy, operational visibility and compliance safeguards. Redundant treatment capacity helps maintain cooling operations during maintenance events, while consistent water quality and discharge performance support efficient, reliable facility operations.

Why is cooling water resilience important for AI and hyperscale data centers? As compute density increases, cooling systems become increasingly critical to operational continuity. Water quality issues, treatment interruptions or equipment failures can affect cooling performance and create operational risk. Resilient cooling water infrastructure helps facilities maintain performance, support efficiency and reduce the likelihood of cooling-related disruptions.

How does redundant data center water treatment reduce operational risk? Redundant data center water treatment systems use parallel filtration and pumping capacity so that individual components can be serviced without interrupting cooling operations. This approach helps reduce single points of failure and supports continuous operation in mission-critical environments where uptime is a priority.

How does cooling water quality affect data center efficiency? Cooling water quality directly influences heat-transfer performance within cooling towers and related equipment. Scale, corrosion and suspended solids can reduce cooling efficiency, increase maintenance requirements and raise operating costs. Effective water treatment helps maintain system performance while supporting long-term cooling reliability.

How do hyperscale data centers maintain discharge compliance while supporting growth? Cooling tower blowdown contains concentrated minerals and trace constituents that may require treatment before discharge. Facilities can support both compliance and operational continuity by integrating treatment processes that consistently meet discharge requirements while accommodating increasing cooling demand as campuses expand.

Redundancy by design: what this Virginia deployment signals for the hyperscale build wave

The most resilient data centers of the future will treat cooling water infrastructure with the same strategic importance as power infrastructure. As AI workloads expand and operational continuity becomes increasingly critical, facilities need cooling systems that can maintain performance through maintenance events, changing operating conditions and continued growth.

The Virginia deployment demonstrates that resilience is not simply about equipment redundancy. It is about creating operational continuity across the entire cooling water lifecycle—from intake and treatment through compliance and discharge. When cooling water infrastructure is designed to support reliability, maintenance flexibility and compliance simultaneously, operators can reduce risk without compromising performance.

As AI accelerates demand for computing capacity, operators are reassessing every dependency that supports uptime. The Northern Virginia project reflects a broader shift across the industry: treating cooling water infrastructure not as a utility system, but as mission-critical infrastructure. For hyperscale campuses, resilience increasingly begins long before the server rack.