Get numbers that count with Flygt Concertor
The intelligent and versatile submersible wastewater pumping solution, proven to deliver exceptional lifecycle value.
It all adds up to exceptional lifecycle value
People working in wastewater deal with numbers every day. Flow volumes. Numbers of callouts. Energy consumption. Inventory levels. And budgets. Xylem’s Flygt Concertor® brings those numbers under control. It adapts in real time, keeps wastewater flowing without interruption, and optimises performance with minimal intervention. By reducing complexity, maintenance requirements and energy consumption, every function works together to deliver exceptional lifecycle value.
Numbers that count today and in the future
Versatile so you can do more with less
Why hold stock you don’t need? Flygt Concertor’s wide operating range means a single pump can cover multiple duty points. Thanks to functions such as adaptive operation and clog detection, components are subjected to less wear over time, helping to reduce the need for replacements. Fewer pumps. Fewer parts. And a much greater likelihood that the right part is on the van when you need it. Altogether, it can reduce inventory by up to 85%*.
Need a scalable solution to meet changing needs?
With Flygt Concertor you are ready for today and tomorrow. It simplifies pump selection today and adapts as your needs evolve.
-
1. Concertor N is a perfect start
Ideal for applications dealing with high volumes of solids and recurring clogging issues. An intelligent standalone pump that can handle a range of flows as communities grow.
-
2. Concertor DP integrates with your algorithms
Add a gateway to easily adjust pump duty and get even more value from your existing process control algorithms. Connect, coordinate, and optimise multiple Flygt Concertor units.
-
3. Concertor XPC is the full system optimiser
Go all in with pump station control that adapts to your station’s needs. Xylem Nexicon® provides advanced functions such as the energy minimiser and sump and pipe cleaning.
Built for continuous flow
Adaptive N® hydraulics allow large solids to pass through without clogging. If a blockage does occur, integrated software detects it and automatically adjusts the pump’s speed and direction of rotation to clear it. The result is fewer service interruptions, fewer site visits, and up to 10x less maintenance costs*.
Sump and pipe cleaning cycles, built into the Nexicon controls, help prevent the build-up of sediment and fats, oils and grease over time. This can reduce vacuum tanker callouts by up to 80%*.
Intelligence that delivers real efficiency
Flygt Concertor pumps have IE4-equivalent motor efficiency that is further enhanced by Xylem Nexicon’s continuous operational analysis. Through real-time adjustments to the optimal duty point and the built-in anti-clogging measures, Flygt Concertor uses the minimum power needed to move wastewater effectively. The result is energy savings of up to 70%*.
Let’s talk about your challenge
No matter the scale or complexity, we’ve seen it before. Share your challenge and let’s talk about overcoming it.
Part of a bigger equation
Flygt Concertor’s performance isn’t just measured in the system, but in the difference it makes above ground. In the way operations run, and in the impact they have on people, communities and the environment.
- Minimising overflows helps protect waterways and avoid costly disruptions.
- Built-in cleaning cycles limit odors and improve conditions for nearby communities.
- Lower energy use and fewer site visits reduce emissions.
- Built-in intelligence limits the need for manual intervention and supports safer working.
Making a difference wherever it goes
See how Flygt Concertor is solving challenges like yours, delivering results across networks worldwide and closer to home.
-
Welsh Water scales up Xylem’s Flygt Concertor for smarter wastewater management
Dŵr Cymru Welsh Water is scaling up its deployment of Flygt Concertor intelligent pumping systems to improve wastewater network resilience, reduce energy consumption, and support its environmental goals.
-
Scottish Water cuts energy by 60% with Flygt Concertor intelligent pump system
Scottish Water partnered with Xylem to upgrade hundreds of pumping stations with innovative, energy-efficient technology, as part of its commitment to reaching net-zero emissions.
-
Flygt Concertor eradicates wastewater pump blockages for Yorkshire Water
Yorkshire Water’s Dynamic Maintenance Team identified that they required an easily deployable solution that delivered tangible benefits across the network.
Check how your numbers could improve
Flygt Concertor is proven to have a measurable impact. Use our handy calculator to see how much you could potentially save by integrating it into your system.
Flygt gives you the value of certainty
With a heritage dating back to 1901, Xylem’s Flygt brand is a recognised leader in the water and wastewater industry. Flygt introduced the world’s first submersible drainage pump in 1947 and the first submersible wastewater pump in 1956. Since then, we have continued to drive innovation, from the self-cleaning N-technology impeller in 1997 to integrated intelligent pump systems in 2016. Today Flygt wastewater pump solutions deliver the value of certainty in more than a million installations worldwide.
*Compared with conventional wastewater pumping systems when utilising the full capabilities of Flygt Concertor®.