It looks like you are coming from United States, but the current site you have selected to visit is Singapore. Do you want to change sites?

Yes, please. No. Keep me on the current site.

How to achieve a truly dry bilge: Xylem’s Rule Dry Bilge Pump explained

June 16, 2026

Even the best-kept boats deal with bilge water. Rough seas, rain, condensation, mast drip, aging hose connections — the sources are many, and the result is the same: water collecting beneath your floorboards, under your engine, and in the tucked-away pockets of your hull. Left unchecked, that standing water becomes the source of mold, mildew, rust, and the all-too-familiar "bilge stink" that no air freshener can truly fix.

The good news: you don't have to accept it. For more than 60 years, Xylem’s Rule brand has been the bilge pump trusted by boaters around the world, and we've built the tools to help you spend time enjoying the water — not worrying about what's sitting beneath your feet.

Why standard bilge pumps can't do the job alone

Most modern boats rely on Rule centrifugal bilge pumps — and for good reason. They move water fast, with some models handling up to 4,000 gallons per hour (more than 15,000 liters per hour) when you need rapid removal. But centrifugal bilge pumps are designed for volume, not for finishing the job. By design, they'll always leave behind roughly ¾ inch (just under 2 cm) of standing water. That residual moisture is all it takes for bacteria, mold, and odor to take hold.

To achieve a genuinely dry, fresh bilge — one that protects your vessel's components, reduces odor at the source, and helps maintain optimal boat performance — you need a second dedicated pump built specifically for that task.

What Is the Rule Dry Bilge Pump?

The Rule Dry Bilge Pump is a self-priming diaphragm pump engineered to remove what your centrifugal pump leaves behind. Unlike submersible bilge pumps, the Rule Dry Bilge Pump is installed above the wet portion of the bilge, which means it can be mounted virtually anywhere — and reach water in areas a traditional pump simply cannot access.

Key specifications and features:

  • Self-priming up to 9.5 ft. (3 m): Creates a strong vacuum to pull remaining water up and out
  • 4 GPM (15 LPM) flow rate: Fast, efficient removal without sacrificing thoroughness
  • Runs dry without damage: No risk to the pump if it catches air before finishing the job
  • Built-in backflow prevention: Stops water from re-entering the bilge during operation
  • 360° rotating pump head and ports: Flexible installation to fit your vessel's layout
  • Compatible with ¾-inch (19 mm) hose barbs and a 90° thru-hull fitting: Works with existing plumbing for a clean, straightforward install

The Dry Bilge Pump removes almost all the water in your bilge, leaving 1/8” (3 mm) or less resulting is a cleaner, drier vessel — and the elimination of bilge stink at its source, without relying on temporary fixes like fragrances or chemical treatments.

See It in action: Tom Nelson tests the Rule Dry Bilge Pump

Angling enthusiast and outdoor broadcaster Tom Nelson takes the Rule Dry Bilge Pump out on the water and walks through exactly how it works alongside a boat's existing pump network. In the video, Tom demonstrates: 

  • How to pair the Rule Dry Bilge Pump with your prevailing centrifugal pump to remove virtually every drop of water from the bilge
  • How to tap into existing onboard wiring for a quick, straightforward installation
  • Real-world performance — what the pump does, how it sounds, and what a dry bilge actually looks like

If you've ever wondered whether the investment in a dedicated dry-bilge solution is worth it, Tom's hands-on walkthrough makes the answer clear. It's the fastest way to understand how these two pump types work together — and why the combination is so effective.

How to eliminate "bilge stink" for good

Standing water in the bilge is the leading cause of unpleasant onboard odors. Bacteria thrives in dark, damp environments, and even a thin layer of residual water is enough to produce the mold and mildew that makes time aboard less enjoyable. The Rule Dry Bilge Pump addresses this at the source — removing moisture before it stagnates, so you're not masking the problem, you're solving it.

Combined with your existing Rule centrifugal pump, it's a complete system: one pump handles volume, the other handles the finish — together protecting your vessel's interior, your onboard equipment, and the overall experience of being on the water.

Easy installation, flexible fit

One of the most practical advantages of the Rule Dry Bilge Pump is its installation flexibility. Because it's not submersible, it mounts above the waterline in the bilge space — accessible, easy to service, and adaptable to a wide range of vessel layouts. The 360° rotating pump head means you can position the inlet and outlet ports to suit your existing hose routing, and connections for ¾-inch (19 mm) hose barbs make integration with most onboard plumbing straightforward.

For most boaters, installation can be completed in a single session using the boat's existing wiring. Tom Nelson's video walks through the process step by step if you want a practical guide before you get started.

The right pump for every bilge challenge

The Rule Dry Bilge Pump is one solution in a full lineup of Rule marine pumps — including electric, manual, engine-driven, automatic, and self-priming options — backed by more than 60 years of marine pumping expertise. Whatever your vessel requires, we're here to help you find the right fit.