It looks like you are coming from United States, but the current site you have selected to visit is China. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Urban drainage resilience: Why drainage has become critical infrastructure

Extreme weather events are increasing across Europe, exposing the limitations of existing sewer and drainage networks. For water utilities and infrastructure operators, having the right operational tools is no longer a strategic choice. It is an operational necessity.

Europe is facing a new climate reality. According to the European Environment Agency (EEA), floods account for 47% of all economic losses associated with extreme weather events across the continent. Between 2020 and 2024, average annual damages reached €44.9 billion, more than five times higher than those recorded during the 1980s.1 In 2024 alone, storms and flooding affected approximately 413,000 people across Europe, causing more than €18 billion in damage.2 From the Rhine basin and Central European plains to the Iberian coastline and Eastern European cities, no region is immune.

For those responsible for managing water services and urban infrastructure, these are not abstract statistics. They represent the operational reality of a challenge that always demands the same urgent response: removing water quickly using the resources available, often under extremely difficult conditions.

The challenge goes beyond water volume

The technical challenge of emergency urban drainage is not simply about managing large volumes of water. It is also about the nature of the fluid itself.

During flooding events, the water entering underpasses, basements, low-lying areas and attenuation tanks is rarely clean. It often contains sediment, suspended solids and a wide variety of debris.

A pump designed for clean water, or one not intended for these operating conditions, may clog, fail or suffer a significant reduction in performance precisely when it is needed most. As a result, pump selection should not be based solely on flow rate (Q) and head (H).

It must also consider real-world operating conditions, including:

  • Fluid composition and solids content
  • Rapid deployment requirements
  • Ease of transport and installation
  • Flexibility across different operating scenarios

During a flood event, the pump must often be operational within minutes, at an unplanned location, and capable of handling water that rarely matches ideal design conditions.

Portability and rapid deployment: critical requirements in emergencies

Emergency drainage operations almost always take place in challenging environments: confined spaces, difficult access points, limited intervention windows and little or no fixed infrastructure.

In these situations, pump portability, the ability to load equipment onto a service vehicle, transport it quickly and commission it without complex auxiliary equipment, often becomes the deciding factor.

Compact stainless-steel submersible pumps are well suited to these applications. Their corrosion-resistant construction helps protect against wastewater and lightly contaminated fluids, while their compact design simplifies transportation and handling. Easy installation reduces response times, and integrated non-return valves help prevent backflow during removal, an important benefit for field teams working under pressure.

Mixed wastewater and solids: when specialist technology is required

Not all drainage scenarios are the same.

While flash floods generally carry varying levels of suspended solids, other applications, including temporary sewer bypasses, pumping station emptying and first-flush management in combined sewer systems, involve a more consistent presence of coarse materials.

For these applications, channel impellers and vortex impellers offer an appropriate technical solution. Their operating principle reduces direct contact between the fluid and the impeller, helping to minimise blockage risks and improve reliability over the long term.

Where larger solids are present, grinder pumps provide an additional level of protection by macerating material before pumping. This enables wastewater to be transported through smaller-diameter pipework, a significant practical advantage when working within existing infrastructure constraints.

From emergency response to resilience planning

Perhaps the most significant change facing utilities today is not technical, but strategic.

When extreme weather events were considered exceptional, emergency drainage equipment could be kept to a minimum and managed on a case-by-case basis. As these events become more frequent, that approach is no longer sufficient.

The question is no longer whether there is a spare pump available. Instead, utilities must develop equipment fleets designed around foreseeable risk scenarios.

Equipment should be selected according to local hydrological conditions and prevailing risk profiles. This means evaluating drainage pumps using the same criteria applied to any other critical infrastructure asset:

  • Reliability under stress
  • Ease of maintenance and serviceability
  • Availability of spare parts
  • Suitability for real operating conditions

This shift also requires investment in operational training, ensuring that personnel can quickly identify, select and deploy the most appropriate solution for each situation.

Equipping maintenance teams with the right resources before an emergency occurs is the only effective strategy when time is no longer on your side.

Lowara solutions

Lowara drainage solutions are designed to support a broad range of emergency drainage and wastewater applications. The range includes:

  • DOC and DIWA series pumps for light sediment applications
  • DOMO pumps for handling suspended solids
  • DOMO GRI grinder pumps for demanding maceration applications

Each solution is engineered for rapid deployment, operational reliability and ease of use in the field.

For further technical specifications, consult the product documentation or contact the technical engineering team.

Elena Ermakova-Fischer
Key Account Manager, Industry & Public Utilities
AW, Xylem

¹ European Environment Agency (EEA) — Economic losses from weather- and climate-related extremes in Europe (2024)
² Copernicus/ECMWF — European State of the Climate 2024: Flooding