It looks like you are coming from United States, but the current site you have selected to visit is Qatar. Do you want to change sites?

Yes, please. No. Keep me on the current site.

How Fond du Lac turned a nutrient mandate into a smarter operating model

Retrofitting for results

When the City of Fond du Lac, Wisconsin, faced stringent phosphorus discharge limits, the wastewater treatment team transformed a tough regulatory mandate into a scalable model for operational resilience. By optimizing existing infrastructure rather than investing in a costly tertiary treatment upgrade, the facility achieved remarkable efficiency.

$82٬000

Annual chemical savings

29%

Energy intensity reduction

Challenge

The regional wastewater treatment facility serves around 75,000 people across the city and 18 neighboring communities. To protect local ecosystems like Lake Winnebago, Wisconsin enforces some of the strictest phosphorus limits in the nation. The utility faced a challenging total phosphorus discharge limit of 0.19 milligrams per liter.

The original system was built to handle ammonia, not deep biological phosphorus removal. Initial efforts to improve phosphorus removal fell short because nitrate concentrations remained too high for the necessary organisms to thrive. The facility needed a new approach to meet regulations without relying on expensive, chemical-heavy processes.

Solution

Having previously partnered with Xylem on energy-saving initiatives, the utility co-developed a smarter, biological treatment retrofit. They implemented CASPERON, Xylem’s advanced simultaneous nitrification-denitrification system. This technology allows ammonia and phosphorus removal to happen in the same tank by creating specific oxygen-rich and oxygen-poor zones.

The team used a phased approach, upgrading one aeration basin at a time. Dense diffuser grids and dynamic aeration controls created spatial oxygen gradients, which suppressed nitrate interference and stabilized the biological process. Now, sensor data feeds directly into automated control systems, adjusting oxygen levels in real time as daily loads fluctuate.

Results

The phased retrofit delivered impressive operational and financial improvements. Between 2018 and 2024, energy consumption dropped by nearly 29 percent. Reliable biological phosphorus removal also led to a sharp decline in chemical use, resulting in over $82,000 in annual chemical savings. Ultimately, the new system paid for itself within two years.

Beyond the financial metrics, plant operators experienced a major shift in their daily work. The team moved from reacting to immediate problems to proactively optimizing the system through sensor maintenance and data monitoring.

"You’ve got to start with what you’ve got. You don’t always need a brand-new system. Sometimes, the answer is to better understand and use what you already have."
Cody Schoepke, Wastewater Superintendent