It looks like you are coming from United States, but the current site you have selected to visit is Croatia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

YSI Biochemistry Customer Applications Guide | Capabilities and Solutions

Patrick Higgins

August 26, 2016
Energy & Power Food & Beverage Life Sciences, Pharma & Biopharma Ammonium Ethanol Glucose Glutamine Lactate Hospitals Analytics

Biochemistry Customer Applications

Through the compilation of numerous end-user profiles, the YSI Customer Applications Guide provides a comprehensive overview of how YSI’s biochemistry analyzers have helped many scientists with their unique applications and uses. With over 40 years of providing rapid, accurate bioanalytical instruments, YSI Life Sciences has established a legacy of expertise in various industrial applications, including, but not limited to:

  • Bioprocess monitoring and control
  • Food & beverage processing and quality control
  • Biofuel research and production
  • Medical and sports physiology research

We hope you will find this guide not only informative but helpful and practical for your real-world analytical needs.

What: The YSI Life Sciences brand represents our series of Biochemistry Analyzers, which feature our innovative biosensor technology. Our analyzers provide critical measurement solutions for pharmaceutical, food & beverage, clinical, industrial, and research applications. YSI Life Sciences analyzers measure a variety of parameters including sugars, alcohols, amino acids, organic acids, electrolytes, and more.

Who: Our customers include pharmaceutical manufacturers, glucometer manufacturers, food processors, biofuel producers, and medical researchers.

Where: Our biochemistry analyzers are used in quality assurance, research laboratories, manufacturing facilities, and hospitals.

Why: Our analyzers are easy to use and cost-effective. Our trusted measurement technology provides rapid, precise, interference-free analysis for our customer’s critical processes.

Because the stakes are always high, our clients choose YSI Life Sciences because of our reputation as the Gold Standard in bioanalytical measurement, our quality products, and our dedication to customer support and service.

YSI Biochemistry Analyzers

Introduction

The following customer profiles represent the various industrial uses and applications of YSI Biochemistry Analyzers by YSI’s United States customers. Many YSI customers were contacted to provide this information. We hope you will find this information useful in assisting you with your particular application.

In many instances, there are numerous customers with the same application. To avoid repetition, applications were only relisted when relatively insightful or different information was uncovered in any of the categories surveyed. For example, there were several customers using a YSI instrument for analyzing sucrose and dextrose in raw potatoes. If their previous methodology, disadvantages, and/or benefits resulted in different or unique information, the application was listed again. By so doing, it is more likely that this document will provide more complete application information and better educate one on the spectrum of benefits attributed to using the YSI bioanalytical technology.

Lastly, the customer profile information will shed light on the disadvantages of alternative methodologies that may be encountered in the field. We hope the information provided here proves useful to you.

Features and Benefits Attributed by End-Users

The following list summarizes customer-provided feedback on the features and benefits of the YSI biochemistry analyzers:

  • Confidence in the quality of the products
  • Rapid results
  • Reliable
  • Reproducible results
  • Economical cost per test
  • Inexpensive to operate
  • Minimal sample preparation
  • Maintain great accuracy – essential for our application
  • Quickly pays for itself
  • Increases productivity
  • High-throughput sample options, i.e., 96-well plate, are a tremendous time saver
  • Results aren’t operator-dependent
  • Optimizes/maximizes production-increases profit
  • Enables us to continually improve our process
  • Offers 2 or more channels for simultaneous measurements
  • Minimal interference sensitivities
  • Accelerates research efforts; moves us more quickly to our research goals; decreases development time
  • Simplifies our job
  • Real-time measurements with rapid results allow us to make adjustments
  • Enables us to pinpoint where in the process the problem has occurred
  • Easily enables us to keep product within quality control specifications and creates a great confidence in the quality of our products while ensuring customers are getting what they pay for
  • Low maintenance, worry-free analyzer
  • Much less reagent preparation
  • Reagents are not toxic
  • Saved us considerable money since we didn’t have to purchase several HPLC’s for remote plants
  • Reagents need not be stored in the freezer
  • Simple to use, easy to train on, user-friendly so you don’t have to be a chemist to use
  • Can use very small sample sizes
  • Labor savings; results are obtained so much more quickly and easier than with other methods
  • Saves time
  • Automated measurements make it easy for students to use
  • Saves money by decreasing wasted product
  • Enhances the work we do
  • Reliable over a wide range of glucose values
  • Autocalibration reduces error
  • Gives us results we would not be able to get otherwise
  • Measures whole blood so it saves time by not having to spin down samples

Bioprocess Customer Profiles

YSI’s bioprocess market is comprised of the biopharmaceutical, biofuels, and industrial biotechnology industries. Each customer profile listed provides a piece of the overall picture of the YSI’s bioprocess market. Lab managers like that YSI analyzers are reliable, provide fast, accurate results, and require minimal operator training.

Several bioprocess applications herein are similar in that they are typically monitoring glucose, a common nutrient source for either mammalian, bacterial or fungal cell cultures. However, there are numerous other nutrients and metabolites that are important to various bioprocesses, and, in turn, require rapid, precise analysis. For example, YSI analyzers measure important nutrients, like glucose, sucrose, and glutamine, and can monitor the level of potentially harmful byproducts, such as lactate and ammonium.

Biopharmaceutical customers employ YSI’s rapid electrode-based measurements to both monitor and control processes. In the biofuels sector, YSI analyzers measure xylose and glucose to monitor fermentation progress in cellulosic ethanol research and measure residual ethanol during distillation in production facilities.

In other applications, real-time monitoring of nutrients, metabolites, and/or product is desirable or even essential. Through the use of YSI’s online monitoring technologies, YSI analyzers are an invaluable tool for real-time analysis of critical nutrients, metabolites, or products – regardless if the process duration spans a few hours or weeks.