It looks like you are coming from United States, but the current site you have selected to visit is Croatia. Do you want to change site?

Yes, please! No, keep me on the current site

Xylem wins innovative technology award from Water Environment Federation

Xylem wins innovative technology award from Water Environment Federation

Award granted for Flygt Experior pump equipped with N-technology and Adaptive impeller

New Orleans, LA – September 30, 2014 – Xylem Inc. (NYSE:XYL), a leading global water technology company dedicated to solving the world's most challenging water issues, has won a 2014 Innovative Technology Award from the Water Environment Federation (WEF) for the company's revolutionary wastewater pumping solution, Flygt Experior.  Flygt Experior's clog-resistant design has been successfully field tested and proven to reduce energy consumption by up to 50 percent, with clog removal maintenance virtually eliminated.  The award will be presented to Xylem at the Water Environment Federation's Annual Technical Exhibition and Conference (WEFTEC), the largest conference of its kind in North America. WEFTEC takes place in the Morial Convention Center, New Orleans, Louisiana, September 27 - October 1, 2014.

Flygt Experior pumps incorporate state-of-the-art N-technology hydraulics, premium efficiency motors and intelligent controls in a package that is simple to install and easy to operate.  These three complementary functions distinguish the fully integrated Flygt Experior system from traditional pump systems.

The muscle of the Flygt Experior is the premium efficiency motor coupled with 'Adaptive N-hydraulics' which further improves the results of the energy-saving, clog-free N-impeller. N-technology is suited for speed regulation as self-cleaning functionality is facilitated independently of rotational speed. Flygt SmartRun controls are pre-programmed with algorithms specifically designed for wastewater systems. The resulting pump performance delivers the ultimate in reliability, efficiency, and simplicity.

The self-cleaning Adaptive N-impeller was recognized by the WEF as the single greatest technology innovation during 2011.  The Adaptive N-impeller moves axially upwards to allow easy passage of trash flow; the impeller then immediately returns to its normal operating position in close proximity to the volute insert ring eliminating clogging even under the most challenging conditions.

The Experior pumping solution now takes the wastewater industry one giant step further. "Extensive field trials in North America and Europe have proven that Flygt Experior only eliminates major clogging problems but also deliver extended service intervals while significantly reducing energy costs," said Lisa Riles, North America Marketing & Business Development Manager, Transport at Xylem Americas.

In Jefferson Parish, LA for instance, four problematic lift stations were retrofitted with one Experior pump each, which completely eliminated clogging problems after startup. Not one instance of pump failure or clogging has occurred. The Experior pumps are coping easily with huge amounts of trash like plastics, rags, baby wipes and straws.

"We are extremely pleased," said Linda Daly, PE, Parish Director of Department of Sewerage. "Despite heavy rains and I&I, we've not had any call outs for pump failures at the four locations that were retrofitted with Flygt Experior systems."

Contact: Louise Cassidy for Xylem

louise.cassidy@edelman.com                                        

Tel +353 (0) 86 383 5727

Xylem