It looks like you are coming from United States, but the current site you have selected to visit is Slovakia. Do you want to change site?

Yes, please! No, keep me on the current site

California Water Board approves Xylem’s ultraviolet disinfection technology: Cutting-edge treatment technology offers new option for expanding water reuse in California

Xylem, (NYSE: XYL), a leading global water technology company dedicated to solving the world's most challenging water issues, announced today that its Wedeco Duron ultraviolet (UV) disinfection system has received conditional acceptance from the California Water Boards' Division of Drinking Water (DDW)*, making it the first UV disinfection system with an inclined lamp array to be available in California for water reuse.

As California continues to suffer from one of the most severe droughts on record, the state continues to look for additional water sources.  Water reuse technology produces high-quality water at a lower life-cycle cost than developing a new water supply. It also delivers a resilient, drought-resistant water source with valuable economic and environmental benefits. 

 

"The Wedeco Duron UV disinfection system is now available to help California address water shortages related to the prolonged drought by cost-efficiently providing purified water for drinking purposes," explained Kirsten Meyer, Product Manager, Xylem. "The Duron UV system provides substantial energy savings compared with conventional systems due to its overall efficiency and adaptability to changing operating conditions, making it an ideal solution to help create a sustainable water supply in California."

 

Water disinfected by Xylem's Wedeco Duron UV system meets the highest standards as required by Title 22 of the California Code of Regulations (CCR) for recycled waters. 

 

Supported by extensive third party validation, Xylem's Wedeco Duron UV system can be fine-tuned to match a customer's water quality, operation conditions and discharge requirements. The innovative design approach ensures that the smallest possible UV system can be installed without compromising performance – saving initial capital costs and operational costs over the life of the system.

 

The Wedeco Duron UV system combines intelligent control with the most advanced UV lamp and ballast technology, ensuring the correct dose and reducing energy consumption by up to 30 percent compared to conventional open channel UV systems**. The unique 600 watt (W) Ecoray UV lamps used in the Wedeco Duron UV system are installed inclined at 45 degrees, which delivers excellent performance and facilitates easy maintenance.

 

* The California Water Board's DDW regulates public water systems, oversees water recycling projects, permits water treatment devices, and supports and promotes water system security.

 

** Based on tests conducted by Carollo Engineers, 2009 (TAK55) and 2014 (Duron). The Wedeco Duron UV disinfection system is validated by the US Environmental Protection Agency (EPA) UV Disinfection Guidance Manual (UVDGM); the National Water Research Institute (NWRI) 2012 Guidelines for Drinking Water and Water Reuse; and the International UV Association (IUVA) uniform protocol for wastewater UV validation applications.

 

About Xylem

 

Xylem (XYL) is a leading global water technology provider, enabling customers to transport, treat, test and efficiently use water in public utility, residential and commercial building services, industrial and agricultural settings. The Company does business in more than 150 countries through a number of market-leading product brands, and its people bring broad applications expertise with a strong focus on finding local solutions to the world's most challenging water and wastewater problems. Xylem is headquartered in Rye Brook, New York, with 2014 revenues of $3.9 billion and approximately 12,500 employees worldwide. Xylem was named to the Dow Jones Sustainability Index for the last four years for advancing sustainable business practices and solutions worldwide and the Company has satisfied the requirements to be a constituent of the FTSE4Good Index Series each year since 2013.

 

The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all – that which occurs in nature. For more information, please visit www.xyleminc.com

 

 

Xylem