It looks like you are coming from United States, but the current site you have selected to visit is Qatar. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Cleaner water, smarter systems, zero disruption

A seven-day transformation at Pro Club

Pro Club, located in Bellevue, Washington, is a premier wellness destination renowned for its state-of-the-art facilities and exceptional service. Spanning a 45,000-gallon main pool and three additional pools, the club serves over 30,000 monthly visitors, offering a pristine environment for health, wellness, and recreation. With its high standards, Pro Club is a hub for influential professionals seeking top-tier amenities and experiences.

Challenge

Despite its reputation for excellence, Pro Club’s aging pool filtration system was no longer meeting the demands of its high-usage facilities. The main pool faced declining water clarity, increased chemical usage, and poor air quality. To maintain its high standards, the club required a swift, high-performance upgrade—one that had to be completed within a tight seven-day window during the holiday break to avoid disrupting members.

Solution

To tackle these challenges, Pro Club partnered with Orca Pacific and Xylem’s Neptune Benson team to implement a cutting-edge solution. The upgrade included Defender® regenerative media filters, which replaced three traditional sand filters, reducing the system footprint by over 50% while capturing particles as small as 1 micron for superior water clarity. Additionally, Wafer® UV disinfection systems were installed, offering a compact and efficient design that significantly improved air quality by reducing chloramines. These systems also featured real-time monitoring capabilities, ensuring seamless operation and maintenance.

Results

The results of the upgrade were transformative for Pro Club. The new system conserves an impressive 520,000 gallons of water annually—enough to fill the main pool 10 times over. Cost savings were equally significant, with annual reductions of $29,000 in water costs, $54,000 in discharge costs, $39,000 in energy bills, $2,000 in chemical costs, and $10,000 in sand replacement. Air quality also saw a dramatic improvement, as chloramine levels were drastically reduced, eliminating harsh odors and creating a more pleasant environment for members. Additionally, the club reclaimed valuable space in the mechanical room, improving operational efficiency and allowing for easier maintenance and future flexibility.

520٬000

gallons of water saved annually

50%+

reduction in system footprint

"The success of this retrofit proves that even the most sophisticated facilities can achieve top-tier upgrades in tight timeframes. With the right partners and technology, transformation is possible."
Orca Pacific Team, Xylem

Conclusion

This seven-day transformation at Pro Club demonstrates the power of smart planning, seamless partnerships, and proven technology. The project not only exceeded performance expectations but also set a new standard for rapid, high-impact upgrades in the aquatics industry.