It looks like you are coming from United States, but the current site you have selected to visit is Malaysia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

HVAC

Building solutions for heating, ventilation & air conditioning systems

areal view  residential houses
WebDAM Path: /Photography & Illustration/Stock Photography/City/Landscape/Building

We spend a large amount of time in buildings. Buildings that are part of an aging infrastructure, buildings that are over 50 years old and equipped with water and heating systems that are outdated, obsolete and inefficient. Collectively, the building environment is the single largest energy consumer in the EU and one of the largest CO2 emitters. Buildings are responsible for 40% of energy consumed and 36% of greenhouse emissions. With a growing population, growing urbanisation, and growing demand for housing, there’s a spiralling need to look closer at how we can change the way we impact climate by adopting sustainable building solutions.

In modern buildings there’s a focus on high comfort at low energy consumption. This means all components, including pumps, must be energy efficient, adapt to the current need and play its part in a big, complex system. Hence why all Xylem products for heating systems are designed to meet and exceed the latest standards regarding energy efficiency and can communicate with modern building systems using for instance Modbus or BACnet.

 

Reducing HVAC Energy Consumption

The deadline’s set: 2030. The goal’s ambitious: net-zero carbon emissions. HVAC has a huge impact on energy efficiency, reducing consumption is a priority.

Modern HVAC systems face the dual challenge of adhering to energy and emission regulations to safeguard the external environment, while ensuring optimal indoor comfort. Almost 40% of a building's energy consumption is attributed to HVAC systems. The adoption of efficient and sustainable heating, ventilation, and air-conditioning technologies plays a pivotal role in decarbonising buildings and achieving the critical goal of net-zero carbon emissions by 2030.

Innovation is powering sustainable technologies, with systems including geothermal heat pumps and solar energy systems working in tandem with district heating networks to create greener energy solutions. Central to the majority of these technologies is the use of hot and cold water cycles to transfer thermal energy.

Regulatory landscape

While the drive to meet that net zero target is strong, buildings cannot reduce their carbon footprints at the expense of safety and related building regulations. The regulations must still be adhered to, which in the case of HVAC include:

  • Directive (EU) 2018/2002 (amending Directive 2012/27/EU) on energy efficiency, which outlines mandatory requirements for remote reading capability for heat metering. This is applicable to systems installed after October 2020.
  • The Energy-Related Products Directive (ErP), which outlines the energy efficiency requirements for all energy-related products. HVAC systems fall under this directive, and to remain compliant they must meet certain energy efficiency standards.

Xylem’s suite of solutions are purposely designed to reduce energy consumption and decarbonise buildings. Created to last, they prevent inefficiency and unnecessary energy usage. Our broad range of products can be tailored in various combinations to create innovative solutions aligned with individual building standards, simultaneously reducing your carbon footprint.

HVAC costs

Cost control is increasingly problematic due to rising energy prices and the need for HVAC systems to face ever-increasing pressure from a changing climate.

The costs associated with HVAC have always represented a substantial investment. Effective systems come at a price, and ongoing maintenance and updates contribute to additional expenses. In recent years, these costs have surged, seemingly exponentially, as an increasingly unpredictable climate places greater demands on HVAC systems. This has led to the need for more frequent maintenance and upgrades and a reduced lifespan for other systems that have needed completely replacing.

Simultaneously, factors such as inflation and rising energy prices contribute to the mounting costs. Effectively combating these challenges involves maximising the use of technological advancements to enhance efficiency and create ecologically and energy-efficient systems.

Efficient cost analysis

While “energy efficiency” may have become a buzzword, it remains a crucial consideration at the core of addressing costs. While the rising awareness of climate change may have propelled it to the forefront of public attention, where cost control is concerned it’s an integral part of creating budget-friendly systems capable of meeting performance needs.

Fortunately, as much as our scientific advancement has cost the planet it has also provided methods of energy conservation and alternatives to fossil fuels, contributing to the creation of energy-efficient and cost-effective systems.

The expenses associated with powering systems are not solely driven by fuel efficiency; various factors influence the costs of running and maintaining HVAC systems. Fortunately, technological advancements allow for more accurate monitoring and analysis of costs, facilitating the ongoing calibration of HVAC systems to run in the most cost-efficient manner moment-to-moment. It also opens the door to developing new ways to reduce costs in the future.          

At Xylem, we offer a range of variable speed packaged booster sets. Upgrading from old, traditional fixed speed systems can result in up to a 70% reduction in energy consumption. Additionally, we provide smart self-integrated pumps and controllers.

Most of our products can be adapted to meet your plants' immediate needs and critical requirements. Discover how Xylem’s solutions can support your approach to HVAC efficiency and cost-effectiveness.

Featured Products & Services

  •  eco2 Residential OEM circulators eco2 Residential OEM circulators eco2 Residential OEM circulators
WebDAM Path: /Photography & Illustration/Products/Lowara

    eco2

    High efficient circulation pump for heating, cooling, domestic hot water, and solar thermal...

Learn more

Enquire about our HVAC solutions