It looks like you are coming from United States, but the current site you have selected to visit is Guyana. Do you want to change site?

Yes, please! No, keep me on the current site

MyConnect or SmartRun Gateway Configuration

Use the Flygt MyConnect Link application to configure the MyConnect or SmartRun Gateway device.

  1. Start the Flygt MyConnect Link application on the computer. The following dialog box opens.
  2. Click the Open a Configuration icon.
  3. Select the Open Default Configuration option.
  4. Click OK.
  5. Go to Connect “MyConnect” > System Setup > Communication.
  6. Enter the Connect ID. (The connect ID is same as Modbus address.)
  7. In the ID Sensitiv list, select Yes.
  8. In the Master or Slave list, select Slave.
  9. Set the master ID number to 1.
  10. Go to Connect “MyConnect” > System Setup > SCADA Setup.
  11. In the SCADA System list, select SYSTEM 2000 60 COMMAND.