It looks like you are coming from United States, but the current site you have selected to visit is Guyana. Do you want to change site?

Yes, please! No, keep me on the current site

Magflux Configuration

The modbus communication module must be installed on the Magflux flowmeter. For more information, see Modbus and RS 485 Communication Module manual.

To prevent noise, disturbance, or traffic into bus line, the Termination switch must be set to ON.

  1. On the Magflux screen, go to Setup Display Setup Modbus COM module/ Communication.

    The Modbus COM module/Communication setting is available when a communication module is connected.
  2. Set the communication parameters.
Parameter Setting
Baud rate 9600
Parity Even
Stop bits 1
Modbus ID offset 000

 

  1. Click OK.
  2. Go to Setup > Display Setup > Network/Modbus
  1. Click Add device.
  2. Select Device 1 or Device 2.
  3. Click OK.
  4. Click Change Device Address.
  5. Select Device 1 or Device 2.
  6. Set the address.
  7. Click OK.
  8. Click Change Display ID No.
  9. Set the number.
  10. Click Number of Displays.
  11. Set the number.
  12. Click OK.
  13. Click Set no. of Retries.
  14. Increase the number by 1.
  15. Click OK.
  16. Change the Modbus speed to low.