It looks like you are coming from United States, but the current site you have selected to visit is Philippines. Do you want to change sites?

Yes, please. No. Keep me on the current site.

EPX Plus Mobile Heater Configuration

The EPX Plus mobile heater comes with an in-built CCD 401 and ready to communicate with Secure Connect. Check the following connections during the initial setup.

CCD 401 EXP Controller RS-485-1
A +
B -
GND GS

 

No configurations are needed for the EPX Plus mobile heater. The user must enter the following values while adding the device in the Secure Connect application.

Parameter Value
Address 1
Data bits 8
Stop bits 1
Parity None
Baud rate 38400