It looks like you are coming from United States, but the current site you have selected to visit is Israel. Do you want to change site?

Yes, please! No, keep me on the current site

APP 411 / APP 412 Configuration

Use the FOP 315 or FOP 402 HMI to configure the APP 411/412 device.

Pump 1 or Mixer 1 must be on node 1, Pump 2 or Mixer 2 must be on node 2, and so on.

  1. Go to Settings Communication.
  2. Select TCP/IP settings or Modbus RTU settings.
  3. Set the communication parameters.
Parameter Setting
IP address 10.10.10.10
Subnet mask 255.255.255.0
Slave address The Modbus address in the network
Baud 9600
Stop bits 1
Parity None
Port 502

A loss in fieldbus communication can stop the pumps. To prevent unexpected pump stops, use the following settings:

Settings Communication > Fieldbus Communication Loss > Action

Put the Action to be on None.