It looks like you are coming from United States, but the current site you have selected to visit is Lebanon. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Release Notes

Avensor, version 1.113 – April 24, 2025

Key features in this release:

  • Phone number validation – users can now validate their phone number in user settings
  • Other minor improvements and work for upcoming features

Avensor, version 1.112 – April 9, 2025

Key features in this release:

  • PSMEGA1 now supported
  • Other minor improvements and work for upcoming features

Avensor, version 1.111 – March 26, 2025

Key features in this release:

  • FPG 413/414 now supports data presentation in Metric, Imperial and USCS

Avensor, version 1.110 – March 12, 2025

Key features in this release:

  • APP 411 now supports data presentation in Metric, Imperial and USCS
  • XCU 411 now shows available asset documentation
  • Alarm lists can now be filtered on device type

Avensor, version 1.109 – February 26, 2025

Key features in this release:

  • MAS 801 now supports data presentation in Metric, Imperial and USCS
  • The weather card now supports rainfall in inches and temperatures in Fahrenheit
  • New device support: Evoqua ATG UV
  • Nexicon can now show accumulated pumped volume in charts instead of only pumped volume per time unit

Avensor, version 1.108 – February 12, 2025

Key features in this release:

  • Nexicon power unit now supports horsepower (hp)
  • Ammonium and potassium as new water quality subcategories now supported for custom device types
  • XCU 411 can now be connected using modbus tcp
  • optimyze now supports data presentation in Metric, Imperial and USCS
  • Fixed an issue with custom device type where you use enumerated values for a data point (category status without subcategory enables enumeration table)

Avensor, version 1.107 – January 29, 2025

Key features in this release:

  • MagFlux volume charts can now show accumulated volume
  • Remote Inspection Kit now supports Carlo Gavazzi EM271 Energy Meter
  • Remote Inspection Kit now has alarms for under/over-range on analog inputs

Avensor, version 1.106 – January 15, 2025

Key features in this release:

  • New device support: PSMEGA2
  • The device SRC 311 can now be used with imperial units (feet, hp)

Avensor, version 1.105 – December 12, 2024

Key features in this release:

  • For stations that have a camera installed, an image archive has been added. In the image archive old snapshots can be viewed. The image archive is located under Station > Devices > Camera
  • The Avensor application’s loading time has significantly improved for users with a suboptimal internet connection.

Avensor, version 1.104 – November 27, 2024

Key features in this release:

  • The optimizely device can now display FFY graphs
  • All stations with a CCD 301 have received a notification warning the user that the CCD 301 reached EOL by May 31, 2025

Avensor, version 1.101 – October 17, 2024

Key features in this release:

  • Addition of new role: Customer View Only (CVO). With similar access as a Service Personnel Read Only, the CVO role is further limited; they cannot acknowledge an alarm or make a note but they can view the station data & alarms.
  • There’s now an option to change CCD IP address in the add station wizard

Avensor, version 1.100 – October 2, 2024

Key features in this release:

  • For the Remote Inspection Kit, it’s now possible to adjust the camera angle, as well as view the current camera online status
  • Device XCU 411 and FPG 413/414 now displays their power, current and speed data in Analytics

Avensor, version 1.98 – September 2, 2024

Key features in this release:

  • Improvement of the data visualization for device PS200

Avensor, version 1.95 – June 20, 2024

Key features in this release:

  • Improved user experience when configuring digital inputs
  • New device support: The device XCU 411 can now be added to Avensor

Avensor, version 1.93 – May 13, 2024

Key features in this release:

  • When a Custom Device Type has a datapoint defined as a valve, the valve is now visualized on the station
  • A Custom Device Type now supports multiple wells