It looks like you are coming from United States, but the current site you have selected to visit is Saudi Arabia. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Features in Xylem Vue Secure Connect

The pillars of Secure Connect are the features that help you monitor your assets. Read more about the different features here.

Features in Xylem Vue Secure Connect

Secure Connect is a digital service that provides alerts and data-driven insights from a device connected to your pump stations or other water infrastructure assets. Once a gateway is installed to connect all the assets, you can have a total overview of all connected operations, anytime, anywhere.

Platform-Wide Features

The Secure Connect platform offers a plug and play monitoring system. Secure Connect connects the supported and the custom devices through Modbus (RS-485, RS-232, or TCP), or analog and digital inputs directly on the CCD 401.

Secure Connect handles the data from multiple stations. Go to the dashboard to get an overview of the station statistics and navigate easily between the stations through a data-driven filtering and sorting.

  • Alarm Management

    Receive real-time data and early warnings from the connected devices.

  • Call Lists

    A call list is a group of users receiving notifications from Secure Connect in case of alarms.

  • Anomaly Detection

    Get notified when a connected device deviates from the expected behavior

  • External Integration

    Connect Secure Connect to other systems through a machine-to-machine API or OPC UA Connector.

Station-Level Features

In Secure Connect, the station is a central concept. Each customer can manage multiple stations, and every station can have sensors, pumps, and other machinery installed. The user can monitor the live data sent by the device such as the status of their assets, or the weather information of your station.

Some devices can be controlled remotely. The user can also can make notes, upload pictures, view the historical data and alarms.

The connected pumps, sensors and other machinery communicate with Secure Connect through a controller, known as a "Device" in Secure Connect. The device is connected to a gateway (CCD 401) that provides the connectivity to Secure Connect. Both devices and gateways require software updates from time to time, which is all managed through Secure Connect.

Incident Monitoring

If a station has no connectivity with Secure Connect, a 'connectivity lost' incident occurs. The incident shows the time period that the connection was lost. Because of system delays, the incidents can have a 30-60 second delay.

In the station analytics, the data and the connectivity lost incidents are collected. This layout makes it possible to correlate the data and a specific incident.

Possible causes can be environmental such as disruptions in the local network or a power outage. It could also be a local issue such as bad radio signal, because of, for example, bad antenna positioning or perhaps the CCD is not connected to the correct antenna port.

To protect your assets the Xylem Network Operations Center monitors the Secure Connect platform 24/7. Additionally Secure Connect's outage detection as well as "Lost contact" alarms keep users informed of the state of their assets.

Questions?

Many users have had similar questions about Events, Alarms, anomalies and incidents.