It looks like you are coming from United States, but the current site you have selected to visit is Ireland. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Prattville addresses treatment capacity and nutrient removal

VertiCel® biological treatment system expands capacity while achieving nitrogen and phosphorus removal limits

Challenge

Nutrient removal is an important process in meeting high quality effluent requirements. Excessive levels of nitrogen and phosphorous disrupt the natural environment and can affect the health of water systems. Furthermore, Prattville's wastewater system was projected to reach its capacity as the population of the surrounding area grew.

Solution

Xylem's VertiCel® System was incorporated into Prattville's wastewater treatment system, which included tanks with fine bubble diffusers, to achieve additional capacity and meet nutrient removal requirements. The VertiCel system uses Xylem's VLR® Vertical Loop Reactors operated in series that allow dissolved oxidation stratification at the front of the process combined with fine bubble tanks at the end of the process to maximize energy efficiency and process flexibility. The VLR reactor tankage is similar to oxidation ditch technology; however, the tanks are flipped on their side with an upper and lower compartment separated by a horizontal baffle.

The VertiCel® Biological Treatment System installed at the Prattville, Alabama wastewater treatment facility was designed to expand treatment capacity and achieve nitrogen and phosphorus removal limits.

Prattville's existing treatment plant consisted of three parallel single reactor aeration basins with a capacity of three million gallons per day (MGD) along with three circular clarifiers. The city selected Xylem's VertiCel Biological Treatment System to expand capacity to 5.7 MGD, while providing the ability to achieve nitrogen and phosphorus removal limits. The VertiCel system was the optimal choice for this upgrade because it allowed the municipality to reuse the existing parallel aeration basins and add fine bubble diffusers. 

Results

Engineers of the South worked closely with Xylem to provide the engineering and design with Brasfield & Gorrie as the general contractors. The project came to Xylem through its partner Jim House & Associates. Commissioning of the plant took place on August 2019 with a ribbon-cutting ceremony and open house.