It looks like you are coming from United States, but the current site you have selected to visit is Ireland. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Evoqua to Provide a Turnkey Wastewater Treatment Solution

An OMNIPAC® SBR field-erected treatment system will be installed to meet infrastructure initiatives for a community in North Carolina

Challenge

​Evoqua Water Technologies has been selected by Carolina Water Service, Inc. of North Carolina, through its sales partner Premier Water, to design, manufacture and install a turnkey wastewater treatment system located in the gated golf course community of Brandywine Bay located in Morehead City, N.C. The plant design will increase reliability, maintain compliance with state regulations, and ensure plant operators' safety. 

Solution

Evoqua will provide a stainless steel OMNIPAC® field-erected sequencing batch reactor (SBR) system designed to treat 0.3 million gallons per day which will replace an existing wastewater treatment system that is nearing the end of its useful life. Evoqua, along with Stroud Engineering from Greenville, North Carolina, provided a thorough evaluation of the existing system and recommended best options for a long-life wastewater treatment solution that would meet total nitrogen limits.

The OMNIPAC®​ SBR Field-Erected Treatment System is a cost-effective, proven advanced wastewater treatment system that can be operational in months instead of years.

Results

The OMNIPAC SBR system is pre-engineered and factory-built providing a less capital-intensive approach to treatment plants than form-built, concrete-basin plants. The design eliminates the need for multiple treatment tanks, separate clarification, and sludge recycle systems requiring less yard piping and easy access to maintenance. The result is a highly flexible and efficient treatment system that can be operational in months instead of years.

Stroud Engineering of Greenville, N.C., worked closely with Evoqua to provide the engineering and design with Jones and Smith Contractors of Winterville, N.C. as the general contractor for this project.