It looks like you are coming from United States, but the current site you have selected to visit is Indonesia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Mobile Treatment Solution Removes PFAS and Other Contaminants from Groundwater

City's sanitary sewer and effluent benefits from contaminant removal at construction site

Project

  • Construction Site Water Treatment

Customer/Stakeholders

  • Environmental Engineering firm in west Michigan
  • Local city officials and government agencies
  • Construction Firm providing excavation and utilities installation

Profile

A city in west Michigan is relocating a 96” sewer main in preparation for future development in the area. The project consists of excavating surface streets to a depth of 25’ below grade. Widely varying volumes of water are seen daily. The project will be completed in several stages over a 6 to 7-month period.

Evoqua Water Technologies was contracted to provide a water treatment solution in addition to the dewatering effort already underway, and connect directly to the well head located at the construction site. The dewatering aspect of the construction project controls the level of groundwater while the treatment aspect mitigates contaminants and metals found in the groundwater.

The system provided was designed to meet 1200 gpm. Each of the media vessels is filled with a proprietary low density granular activated carbon.

The contaminants being targeted include PFAS. Among the targeted volatile organic compounds (VOCs) are benzene, toluene, xylenes, methylene chloride and others. Evoqua’s media is also removing many types of metals including arsenic, barium, cadmium, lead and others. In addition, pH is a challenge due to significant fluctuations.

The treated effluent is being discharged into the city’s sanitary sewer system.

Equipment

  • Media vessels
  • Bag Filtration to .5µm absolute
  • Frac Tanks providing equalization and solids settling
  • UC1240LD activated carbon