It looks like you are coming from United States, but the current site you have selected to visit is Bahrain. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode
< View all Making Connections
Unlock the Hidden Potential of Ultrasonic Metering

Unlock the Hidden Potential of Ultrasonic Metering

Imagine a world where your gas meters are more than just passive data collectors. A world where they actively monitor, analyze, and respond to situations in near real-time, ensuring optimal performance and efficiency. With ultrasonic metering, your utility can unlock cutting-edge technology to ensure intelligent decision-making at the edge.

At the heart of this revolution lies the Sonix IQ, a game-changing ultrasonic meter that redefines the boundaries of what a gas meter can do. With its advanced electronics and integrated sensors, the Sonix IQ transforms from a mere data point into a powerful edge intelligence hub.

Let's dive into the hidden benefits that set ultrasonic metering apart:

Unparalleled Accuracy and Longevity: Say goodbye to the days of drifting metrology accuracy and worn-out moving parts. Ultrasonic meters like the Sonix IQ boast a design free from mechanical components, ensuring precise measurements throughout their lifespan. Couple that with enhanced temperature correction capabilities, and you've got a meter that consistently delivers high-resolution data, for the entirety of its 20-year battery life.

Edge Intelligence: The future is now because ultrasonic metering goes beyond simple data collection. With integrated electronics and intelligent software, the Sonix IQ has become a true edge intelligence platform. Imagine a meter that can seamlessly integrate with a shutoff valve, pressure sensor, temperature sensor, and more. This synergy empowers the meter to make informed decisions at the point of data collection, triggering alarms or initiating shutoffs in emergency situations – all without relying on input from a head-end system or a user driving out to manually shut off the meter.

Enhanced Communication and Health Monitoring: Bidirectional communication is the name of the game with ultrasonic meters like the Sonix IQ. With an integrated radio (only with FlexNet), you can request data, initiate shutoffs, or even push firmware updates over the air. But that's not all – these intelligent meters continuously run self-diagnostics, actively monitoring their health and accuracy. If any issues arise, such as reverse flow, air in the meter, or low battery voltage, the meter will promptly communicate the problem, ensuring proactive maintenance and minimizing downtime.

Data Logging and Alarm Management: Even in the absence of a radio, the Sonix IQ has your back. With its robust data logging capabilities, the meter stores up to 90 days' worth of data and alarms, ensuring valuable information is never lost. This wealth of data not only provides insights into meter performance but also aids in detecting and addressing potential issues promptly.

In the ever-evolving landscape of energy management, ultrasonic metering is more than just a technological advancement – it's a paradigm shift. By embracing the power of edge intelligence, enhanced communication, and unrivaled accuracy, utilities can unlock new levels of efficiency, sustainability, and customer satisfaction.

So, why settle for ordinary when you can harness the hidden potential of ultrasonic metering? Dive into the future today and experience the game-changing benefits of the Sonix IQ and its ultrasonic counterparts. 

;