It looks like you are coming from United States, but the current site you have selected to visit is Ireland. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Adding a preventative maintenance program to Yorkshire Water’s 15-year-old Wedeco UV disinfection systems at eight treatment plants reduced callouts by almost 70%.

Targeted disinfection is a crucial part of the wastewater treatment process, hence why Yorkshire Water has been operating Xylem’s Wedeco TAK 55 UV disinfection systems for more than 15 years.

The modularly designed system allows practically unlimited quantities of wastewater to be disinfected, with 100% safety and energy efficiency.

Download Case study