It looks like you are coming from United States, but the current site you have selected to visit is China. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Enable high contrast mode

Flygt流道式叶轮泵

C-3000

流道式叶轮泵

  • 无堵塞叶轮
  • 单叶片和多叶片设计
  • 传统大通孔设计
  • 净水效率高
  • ​铸铁和可选的叶轮材料

需要帮助吗?

联系专家

Contact an Expert

Whether you would like additional information or are interested in getting a quote, we're here to help.

All fields required.

*  必填字段
Product Models 技术 案例研究 & 和白皮书
Product Models
没有结果与您的搜索匹配
技术

FLYGT流道式叶轮泵

流道式叶轮C型泵用于处理流速达3000 l/s(48000gpm)的介质,使用的电动机功率达775 kW(1050 hp)。这些泵的基础型号采用耐用铸铁制成,专用于高要求应用场合,比如处理城市污水和工业废水。提供防爆型号。经典C型泵,配备闭式单叶片和多叶片叶轮已经受住多年的考验。较小C型泵配备Flygt Nevaclog®叶轮,具有较大的固体通过自由通道。较大泵配备多叶片叶轮,具有最大的液压效率和抗堵塞性。

案例研究 & 和白皮书

Circular stormwater pump station

FRANCE

Challenge One of the largest airports serving France required a stormwater treatment plant to handle the inflow from a large gravity sewer collecting water from the runways. Solution The pump station...

阅读更多内容

Pump station with cleaning function

SWEDEN

Challenge Eighteen Flygt pump stations transport wastewater at a popular recreational and amusement area in central Stockholm. One of the pump stations handles restaurant wastewater containing fats,...

阅读更多内容

Expansion of a desalination plant

AUSTRALIA

Challenge One of Australia’s largest cities was running short of fresh water and needed a major expansion of its desalination facility. One hurdle was to transfer the seawater to the plant. A new...

阅读更多内容

Large capacity circular wet well

USA

Challenge Very deep, large capacity and limited footprint: these are common demands by customers for their pump stations designs. Recently, two such pump stations were needed in the US. Solution The...

阅读更多内容

Circular wastewater lift station

USA

Challenge A 54,000-acre service area in a major city in Texas required assistance to handle a projected 50% increase in population and subsequent increase in wastewater processing demands. Solution...

阅读更多内容