It looks like you are coming from United States, but the current site you have selected to visit is Venezuela. Do you want to change site?

Yes, please! No, keep me on the current site

Bombas con impulsor de canal Flygt

C-3000

BOMBAS CON IMPULSOR DE CANAL

  • Impulsores antiatasco
  • Diseños con uno o varios álabes
  • Diseños tradicionales con secciones de paso grandes
  • Altas eficiencias con agua limpia
  • Hierro fundido y materiales opcionales para el impulsor

Need help?

Contact an Expert

Solicitar información

Si desea información adicional o está interesado en recibir una oferta, estamos aquí para ayudarle.

All fields required.

*  Required Field
Pump Models Technology Case Studies & White Papers
Pump Models
There are no results that match your search
Technology

BOMBAS CON IMPULSOR DE CANAL FLYGT

Flygt Las bombas C con impulsor de canal están fabricadas para manejar capacidades de hasta 3000 l/s (48.000 gpmgpm) con motores de hasta 775 kW (1050 hp). Las versiones básicas de estas bombas están fabricadas con hierro fundido de gran duración y están destinadas a aplicaciones exigentes como el alcantarillado municipal y los efluentes industriales. Hay versiones a prueba de explosión disponibles. Las bombas C clásicas con impulsores cubiertos con uno o varios vanos han demostrado su rendimiento durante muchos años. Las bombas C más pequeñas cuentan con el impulsor Flygt Nevaclog®, que ofrece propiedades de paso de sólidos gracias a su gran paso libre. Las bombas más grandes cuentan con impulsores de varios vanos para ofrecer la máxima eficiencia hidráulica y resistencia frente a atascos.

Case Studies & White Papers

Circular stormwater pump station

FRANCE

Challenge One of the largest airports serving France required a stormwater treatment plant to handle the inflow from a large gravity sewer collecting water from the runways. Solution The pump station...

Read More

Pump station with cleaning function

SWEDEN

Challenge Eighteen Flygt pump stations transport wastewater at a popular recreational and amusement area in central Stockholm. One of the pump stations handles restaurant wastewater containing fats,...

Read More

Expansion of a desalination plant

AUSTRALIA

Challenge One of Australia’s largest cities was running short of fresh water and needed a major expansion of its desalination facility. One hurdle was to transfer the seawater to the plant. A new...

Read More

Sewage and stormwater pump stations

UK

Storm water pump station design Challenge The revival of one of Britain’s largest commercially unexploited land areas called for multi-phase construction of two large pump stations. One pump station...

Read More

Large capacity circular wet well

USA

Challenge Very deep, large capacity and limited footprint: these are common demands by customers for their pump stations designs. Recently, two such pump stations were needed in the US. Solution The...

Read More

Circular wastewater lift station

USA

Challenge A 54,000-acre service area in a major city in Texas required assistance to handle a projected 50% increase in population and subsequent increase in wastewater processing demands. Solution...

Read More